PLVideoWriter.CompressionModeEnum Class#
Visibility: Beginner
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLVideoWriter.CompressionModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLVideoWriter.CompressionModeEnum | Initializes a new instance of the PLVideoWriter.CompressionModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Bitrate | The resulting stream has a constant bit rate. | |
名前 | The full name of CompressionMode (Overrides ParameterListEnum.Name.) | |
Quality | The resulting stream has a constant quality. |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of CompressionMode (Overrides Object.ToString()()()().) |
PLVideoWriter.CompressionModeEnum.ToString Method#
The full name of CompressionMode
Return Value#
Type: String
Returns the full name of CompressionMode
PLVideoWriter.CompressionModeEnum Constructor#
Initializes a new instance of the PLVideoWriter.CompressionModeEnum class
PLVideoWriter.CompressionModeEnum.Bitrate Property#
The resulting stream has a constant bit rate.
PLVideoWriter.CompressionModeEnum.Name Property#
The full name of CompressionMode
PLVideoWriter.CompressionModeEnum.Quality Property#
The resulting stream has a constant quality.