IGrabResult Interface#
Syntax#
C#
VB
The IGrabResult type exposes the following members.
プロパティ#
名前 | 説明 | |
---|---|---|
BlockID | The block ID of the grabbed frame. The format of the value depends on the camera device used. | |
BufferUserData | Get the pointer of the buffer context retrieved when calling AllocateBuffer(Int64, Object, IntPtr, Object). | |
ChunkData | The collection of attached chunk data. | |
Container | Retrieves the container with the data components. | |
ErrorCode | The error code generated when an image cannot be grabbed successfully (GrabSucceeded is false). | |
ErrorDescription | Description of the error generated when an image cannot be grabbed successfully (GrabSucceeded is false). | |
GrabSucceeded | Indicates if an image has been grabbed successfully. | |
HasChunkData | Indicates if chunk data is available. | |
HasCRC | Indicates if the buffer has a CRC checksum attached. A CRC checksum needs to be activated for the camera device. See the PayloadCRC16 chunk. | |
Height | The height of the image in pixels, i.e. the number of image rows. (Inherited from IImage.) | |
ID | The ID of the grabbed image. | |
ImageNumber | The number of the image. | |
IsValid | Indicates if the image is valid. (Inherited from IImage.) | |
OffsetX | Horizontal offset from the left side of the sensor to the image ROI. | |
OffsetY | Vertical offset from the top of the sensor to the image ROI. | |
Orientation | The vertical orientation of the pixel data stored in memory. (Inherited from IImage.) | |
PaddingX | The number of data bytes added to the end of each row. (Inherited from IImage.) | |
PaddingY | The number of data bytes added to the end of the image data. | |
PayloadSize | The current payload size in bytes. | |
PayloadTypeValue | The payload type. | |
PixelData | The pixel data buffer. The type of the object containing the buffer depends on the class implementing this interface. The pixel data buffer is provided as a byte array if no custom buffer factory is used. With a custom buffer factory the provided type is dependent on its specific implementation. (Inherited from IImage.) | |
PixelDataPointer | The pointer to the pixel data buffer. (Inherited from IImage.) | |
PixelTypeValue | The pixel type. (Inherited from IImage.) | |
SkippedImageCount | The number of images that were skipped before this image was acquired. | |
StreamGrabberUserData | The UserData value assigned to the stream grabber object. | |
Timestamp | The camera specific tick count. | |
Width | The width of the image in pixels, i.e. the number of image columns. (Inherited from IImage.) |
方法#
名前 | 説明 | |
---|---|---|
CheckCRC | Indicates if the CRC checksum of the buffer is valid. | |
Clone | Clones the grab result for distribution of the grab result data to different modules. All clones must be disposed. The cloned grab result references the same grab result data. No grab result data is copied. |
Extension Methods#
名前 | 説明 | |
---|---|---|
ComputeStride | Computes the stride of the image in bytes. Returns null if the stride cannot be computed. (Defined by IImageExtensions.) | |
画面 | Uses the ImageWindow method DisplayImage(Int32, IImage) to display the image. (Defined by IImageExtensions.) |
Remarks#
The grab result controls the reuse and the lifetime of the referenced pixel data buffer. If the original and all cloned grab results referencing a pixel data buffer are disposed, the pixel data buffer is freed or reused by the camera stream grabber (depending on the used buffer type). The data and the pixel data buffer are still valid after the original camera object has been disposed.
Caution |
---|
If the grab results are never disposed, the grabbing will stop with an input queue underrun. |
IGrabResult.CheckCRC Method#
Indicates if the CRC checksum of the buffer is valid.
Syntax#
C#
VB
Return Value#
Type: Boolean
Returns true if the CRC checksum is valid.
Remarks#
Error Safety:
Does not throw exceptions.
IGrabResult.Clone Method#
Clones the grab result for distribution of the grab result data to different modules. All clones must be disposed. The cloned grab result references the same grab result data. No grab result data is copied.
Syntax#
C#
VB
Return Value#
Type: IGrabResult
Returns a new grab result referencing the same grab result data.
Remarks#
Caution |
---|
If the grab results are never disposed, the grabbing will stop with an input queue underrun. |
Can throw exceptions.
IGrabResult.BlockID Property#
The block ID of the grabbed frame. The format of the value depends on the camera device used.
Syntax#
C#
VB
Property Value#
Type: Int64
Remarks#
GigE Camera Devices: The sequence number starts with 1 and wraps at 65535. The value 0 indicates that this feature is not supported by the camera.
USB camera devices: The sequence number starts with 0 and uses the full 64 bit range.
Attention:
A block ID with the value UINT64_MAX indicates that the block ID is invalid and must not be used.
IGrabResult.BufferUserData Property#
Get the pointer of the buffer context retrieved when calling AllocateBuffer(Int64, Object, IntPtr, Object).
Syntax#
C#
VB
Property Value#
Type: Object
Remarks#
Error Safety:
Does not throw exceptions.
IGrabResult.ChunkData Property#
The collection of attached chunk data.
Syntax#
C#
VB
Property Value#
Type: IParameterCollection
Remarks#
The returned collection can be empty.
Error Safety:
Does not throw exceptions.
IGrabResult.Container Property#
Retrieves the container with the data components.
Syntax#
C#
VB
Property Value#
Type: IDataContainer
Remarks#
Any grab result containing an image can create a data container. Some cameras can return grab results consisting of multiple components.
Preconditions: The grab result must be valid.
Error Safety: Does throw exceptions.
IGrabResult.ErrorCode Property#
The error code generated when an image cannot be grabbed successfully (GrabSucceeded is false).
Syntax#
C#
VB
Property Value#
Type: Int32
Remarks#
Error Safety:
Does not throw exceptions.
IGrabResult.ErrorDescription Property#
Description of the error generated when an image cannot be grabbed successfully (GrabSucceeded is false).
Syntax#
C#
VB
Property Value#
Type: String
Remarks#
Error Safety:
Does not throw exceptions.
IGrabResult.GrabSucceeded Property#
Indicates if an image has been grabbed successfully.
Syntax#
C#
VB
Property Value#
Type: Boolean
Remarks#
Error Safety:
Does not throw exceptions.
IGrabResult.HasChunkData Property#
Indicates if chunk data is available.
Syntax#
C#
VB
Property Value#
Type: Boolean
Remarks#
This is the case if: a) the chunk mode is enabled for the camera device, b) the parameter ChunkNodeMapsEnable of the camera object is set to true (default setting), c) chunk data node maps are supported by the transport layer of the camera device.
Error Safety:
Does not throw exceptions.
IGrabResult.HasCRC Property#
Indicates if the buffer has a CRC checksum attached. A CRC checksum needs to be activated for the camera device. See the PayloadCRC16 chunk.
Syntax#
C#
VB
Property Value#
Type: Boolean
Remarks#
Error Safety:
Does not throw exceptions.
IGrabResult.ID Property#
The ID of the grabbed image.
Syntax#
C#
VB
Property Value#
Type: Int64
Remarks#
Always returns a number larger than 0. The counting starts with 1 and is never reset during the lifetime of the Instant Camera object.
Error Safety:
Does not throw exceptions.
IGrabResult.ImageNumber Property#
The number of the image.
Syntax#
C#
VB
Property Value#
Type: Int64
Remarks#
Error Safety:
Does not throw exceptions.
IGrabResult.OffsetX Property#
Horizontal offset from the left side of the sensor to the image ROI.
Syntax#
C#
VB
Return Value#
Type: Int32
Horizontal offset from the left side of the sensor to the image ROI. This specifies the position of the image ROI. Only defined if the grab result contains image data.
Remarks#
Error Safety:
Does not throw exceptions.
IGrabResult.OffsetY Property#
Vertical offset from the top of the sensor to the image ROI.
Syntax#
C#
VB
Return Value#
Type: Int32
Vertical offset from the top of the sensor to the image ROI. This specifies the position of the image ROI. Only defined if the grab result contains image data.
Remarks#
Error Safety:
Does not throw exceptions.
IGrabResult.PaddingY Property#
The number of data bytes added to the end of the image data.
Syntax#
C#
VB
Property Value#
Type: Int32
Remarks#
Error Safety:
Does not throw exceptions.
IGrabResult.PayloadSize Property#
The current payload size in bytes.
Syntax#
C#
VB
Property Value#
Type: Int64
Remarks#
Error Safety:
Does not throw exceptions.
IGrabResult.PayloadTypeValue Property#
The payload type.
Syntax#
C#
VB
Property Value#
Type: PayloadType
Remarks#
Error Safety:
Does not throw exceptions.
IGrabResult.SkippedImageCount Property#
The number of images that were skipped before this image was acquired.
Syntax#
C#
VB
Return Value#
Type: Int64
Always returns a number larger than or equal 0. This number does not include the number of images lost in case of a buffer underrun in the driver.
Remarks#
Error Safety:
Does not throw exceptions.
IGrabResult.StreamGrabberUserData Property#
The UserData value assigned to the stream grabber object.
Syntax#
C#
VB
Property Value#
Type: Object
Remarks#
The UserData of the stream grabber is attached to the grab result when the grab result is retrieved.
Error Safety:
Does not throw exceptions.
IGrabResult.Timestamp Property#
The camera specific tick count.
Syntax#
C#
VB
Property Value#
Type: Int64
Remarks#
The tick count indicates when the image exposure was started. Cameras that do not support this feature return zero. If supported, this can be used to determine which image AOIs were acquired simultaneously.
Error Safety:
Does not throw exceptions.