PLCamera.CxpLinkConfigurationPreferredEnum Class#
Applies to: boost CoaXPress and boost_V_CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.CxpLinkConfigurationPreferredEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.CxpLinkConfigurationPreferredEnum | Initializes a new instance of the PLCamera.CxpLinkConfigurationPreferredEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Auto | The link configuration is set to automatic discovery. Applies to: boost CoaXPress | |
CXP10_X1 | The link configuration is set to 1 connection operating at CXP-10 speed (10 Gbps). Applies to: boost CoaXPress | |
CXP10_X2 | The link configuration is set to 2 connections operating at CXP-10 speed (10 Gbps). Applies to: boost CoaXPress | |
CXP12_X1 | The link configuration is set to 1 connection operating at CXP-12 speed (12.5 Gbps). Applies to: boost CoaXPress and boost_V_CoaXPress | |
CXP12_X2 | The link configuration is set to 2 connections operating at CXP-12 speed (12.5 Gbps). Applies to: boost CoaXPress and boost_V_CoaXPress | |
CXP12_X4 | The link configuration is set to 4 connections operating at CXP-12 speed (12.5 Gbps). Applies to: boost_V_CoaXPress | |
CXP2_X1 | The link configuration is set to 1 connection operating at CXP-2 speed (2.5 Gbps). Applies to: boost CoaXPress | |
CXP2_X2 | The link configuration is set to 2 connections operating at CXP-2 speed (2.5 Gbps). Applies to: boost CoaXPress | |
CXP3_X1 | The link configuration is set to 1 connection operating at CXP-3 speed (3.125 Gbps). Applies to: boost CoaXPress | |
CXP3_X2 | The link configuration is set to 2 connections operating at CXP-3 speed (3.125 Gbps). Applies to: boost CoaXPress | |
CXP5_X1 | The link configuration is set to 1 connection operating at CXP-5 speed (5 Gbps). Applies to: boost CoaXPress | |
CXP5_X2 | The link configuration is set to 2 connections operating at CXP-5 speed (5 Gbps). Applies to: boost CoaXPress | |
CXP6_X1 | The link configuration is set to 1 connection operating at CXP-6 speed (6.25 Gbps). Applies to: boost CoaXPress | |
CXP6_X2 | The link configuration is set to 2 connections operating at CXP-6 speed (6.25 Gbps). Applies to: boost CoaXPress and boost_V_CoaXPress | |
CXP6_X4 | The link configuration is set to 4 connections operating at CXP-6 speed (6.25 Gbps). Applies to: boost_V_CoaXPress | |
名前 | The full name of CxpLinkConfigurationPreferred (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of CxpLinkConfigurationPreferred (Overrides Object.ToString()()()().) |
PLCamera.CxpLinkConfigurationPreferredEnum.ToString Method#
The full name of CxpLinkConfigurationPreferred
Return Value#
Type: String
Returns the full name of CxpLinkConfigurationPreferred
PLCamera.CxpLinkConfigurationPreferredEnum Constructor#
Initializes a new instance of the PLCamera.CxpLinkConfigurationPreferredEnum class
PLCamera.CxpLinkConfigurationPreferredEnum.Auto Property#
The link configuration is set to automatic discovery.
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP10_X1 Property#
The link configuration is set to 1 connection operating at CXP-10 speed (10 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP10_X2 Property#
The link configuration is set to 2 connections operating at CXP-10 speed (10 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP12_X1 Property#
The link configuration is set to 1 connection operating at CXP-12 speed (12.5 Gbps).
Applies to: boost CoaXPress and boost_V_CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP12_X2 Property#
The link configuration is set to 2 connections operating at CXP-12 speed (12.5 Gbps).
Applies to: boost CoaXPress and boost_V_CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP12_X4 Property#
The link configuration is set to 4 connections operating at CXP-12 speed (12.5 Gbps).
Applies to: boost_V_CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP2_X1 Property#
The link configuration is set to 1 connection operating at CXP-2 speed (2.5 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP2_X2 Property#
The link configuration is set to 2 connections operating at CXP-2 speed (2.5 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP3_X1 Property#
The link configuration is set to 1 connection operating at CXP-3 speed (3.125 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP3_X2 Property#
The link configuration is set to 2 connections operating at CXP-3 speed (3.125 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP5_X1 Property#
The link configuration is set to 1 connection operating at CXP-5 speed (5 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP5_X2 Property#
The link configuration is set to 2 connections operating at CXP-5 speed (5 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP6_X1 Property#
The link configuration is set to 1 connection operating at CXP-6 speed (6.25 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP6_X2 Property#
The link configuration is set to 2 connections operating at CXP-6 speed (6.25 Gbps).
Applies to: boost CoaXPress and boost_V_CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP6_X4 Property#
The link configuration is set to 4 connections operating at CXP-6 speed (6.25 Gbps).
Applies to: boost_V_CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.Name Property#
The full name of CxpLinkConfigurationPreferred