PLTransportLayer.LutEnableEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.LutEnableEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLTransportLayer.LutEnableEnum | Initializes a new instance of the PLTransportLayer.LutEnableEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of LutEnable (Overrides ParameterListEnum.Name.) | |
Off | The trigger queue mode is disabled. Applies to: CoaXPress | |
その | The trigger queue mode is enabled. Applies to: CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of LutEnable (Overrides Object.ToString()()()().) |
PLTransportLayer.LutEnableEnum.ToString Method#
The full name of LutEnable
Return Value#
Type: String
Returns the full name of LutEnable
PLTransportLayer.LutEnableEnum Constructor#
Initializes a new instance of the PLTransportLayer.LutEnableEnum class
PLTransportLayer.LutEnableEnum.Name Property#
The full name of LutEnable
PLTransportLayer.LutEnableEnum.Off Property#
The trigger queue mode is disabled.
Applies to: CoaXPress
PLTransportLayer.LutEnableEnum.On Property#
The trigger queue mode is enabled.
Applies to: CoaXPress