CommandName Structure#
Syntax#
C#
VB
The CommandName type exposes the following members.
Constructors#
名前 | 説明 | |
---|---|---|
CommandName | Create a command parameter name. |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | Returns the command parameter name as string. |
方法#
名前 | 説明 | |
---|---|---|
ToString | Returns the command parameter name as string. (Overrides ValueType.ToString().) |
Operators#
名前 | 説明 | |
---|---|---|
Explicit(String to CommandName) | A cast can be used to create a command parameter name from a string. |
CommandName Explicit Conversion (String to CommandName)#
A cast can be used to create a command parameter name from a string.
Syntax#
C#
VB
パラメーター#
- name
- Type: System.String
The name of the parameter as string. The name can include path information.
Return Value#
Type: CommandName
Returns the command parameter name.
CommandName.ToString Method#
Returns the command parameter name as string.
Syntax#
C#
VB
Return Value#
Type: String
Returns the command parameter name as string. The name can include path information.
CommandName Constructor#
Create a command parameter name.
Syntax#
C#
VB
パラメーター#
- name
- Type: System.String
The name of the parameter as string. The name can include path information.
CommandName.Name Property#
Returns the command parameter name as string.
Syntax#
C#
VB
Property Value#
Type: String
CommandName Type Conversions#
The CommandName type exposes the following members.
Operators#
名前 | 説明 | |
---|---|---|
Explicit(String to CommandName) | A cast can be used to create a command parameter name from a string. |