PLCamera.DeviceTemperatureSelectorEnum Class#
Applies to: CamEmu, ace 2 GigE, ace 2 USB, ace USB, blaze, boost CoaXPress, boost_V_CoaXPress and dart 2 USB
Visibility: Expert
Selecting Parameters: DeviceTemperature
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.DeviceTemperatureSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.DeviceTemperatureSelectorEnum | Initializes a new instance of the PLCamera.DeviceTemperatureSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
カメラ | The temperature is measured on the camera housing. Applies to: boost CoaXPress | |
Coreboard | The temperature is measured on the core board. Applies to: CamEmu, ace 2 GigE, ace 2 USB and ace USB | |
CPU | Temperature of the device's CPU. Applies to: blaze | |
FpgaCore | The temperature is measured on the FPGA board. Applies to: boost CoaXPress, boost_V_CoaXPress and dart 2 USB | |
Framegrabberboard | The temperature is measured on the frame grabber board. Applies to: ace USB | |
照明 | Temperature of the device's illumination board. Applies to: blaze | |
名前 | The full name of DeviceTemperatureSelector (Overrides ParameterListEnum.Name.) | |
Sensor | The temperature is measured on the image sensor. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Sensorboard | The temperature is measured on the sensor board. Applies to: ace USB and blaze |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of DeviceTemperatureSelector (Overrides Object.ToString()()()().) |
PLCamera.DeviceTemperatureSelectorEnum.ToString Method#
The full name of DeviceTemperatureSelector
Return Value#
Type: String
Returns the full name of DeviceTemperatureSelector
PLCamera.DeviceTemperatureSelectorEnum Constructor#
Initializes a new instance of the PLCamera.DeviceTemperatureSelectorEnum class
PLCamera.DeviceTemperatureSelectorEnum.Camera Property#
The temperature is measured on the camera housing.
Applies to: boost CoaXPress
PLCamera.DeviceTemperatureSelectorEnum.Coreboard Property#
The temperature is measured on the core board.
Applies to: CamEmu, ace 2 GigE, ace 2 USB and ace USB
PLCamera.DeviceTemperatureSelectorEnum.CPU Property#
Temperature of the device's CPU.
Applies to: blaze
PLCamera.DeviceTemperatureSelectorEnum.FpgaCore Property#
The temperature is measured on the FPGA board.
Applies to: boost CoaXPress, boost_V_CoaXPress and dart 2 USB
PLCamera.DeviceTemperatureSelectorEnum.Framegrabberboard Property#
The temperature is measured on the frame grabber board.
Applies to: ace USB
PLCamera.DeviceTemperatureSelectorEnum.Illumination Property#
Temperature of the device's illumination board.
Applies to: blaze
PLCamera.DeviceTemperatureSelectorEnum.Name Property#
The full name of DeviceTemperatureSelector
PLCamera.DeviceTemperatureSelectorEnum.Sensor Property#
The temperature is measured on the image sensor.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.DeviceTemperatureSelectorEnum.Sensorboard Property#
The temperature is measured on the sensor board.
Applies to: ace USB and blaze