PLPixelDataConverter.OutputBitAlignmentEnum Class#
Visibility: Beginner
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLPixelDataConverter.OutputBitAlignmentEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLPixelDataConverter.OutputBitAlignmentEnum | Initializes a new instance of the PLPixelDataConverter.OutputBitAlignmentEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
LsbAligned | Image data is aligned with the least significant bit. | |
MsbAligned | Image data is aligned with the most significant bit. | |
名前 | The full name of OutputBitAlignment (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of OutputBitAlignment (Overrides Object.ToString()()()().) |
PLPixelDataConverter.OutputBitAlignmentEnum.ToString Method#
The full name of OutputBitAlignment
Return Value#
Type: String
Returns the full name of OutputBitAlignment
PLPixelDataConverter.OutputBitAlignmentEnum Constructor#
Initializes a new instance of the PLPixelDataConverter.OutputBitAlignmentEnum class
PLPixelDataConverter.OutputBitAlignmentEnum.LsbAligned Property#
Image data is aligned with the least significant bit.
PLPixelDataConverter.OutputBitAlignmentEnum.MsbAligned Property#
Image data is aligned with the most significant bit.
PLPixelDataConverter.OutputBitAlignmentEnum.Name Property#
The full name of OutputBitAlignment