GenApiノードのPtrクラス#
ファイル#
名前 |
---|
GenApi/Pointer.h Definition of template CPointer. |
GenApi/Types.h Common types used in the public GenApi interface. |
クラス#
名前 | |
---|---|
class | GenApi::CPointer Encapsulates a GenApi pointer dealing with the dynamic_cast automatically. |
class | GenApi::CFloatPtr SmartPointer for IFloat interface pointer. |
タイプ#
名前 | |
---|---|
enum | _ESign |
enum | _EAccessMode |
enum | _EVisibility |
enum | _ECachingMode |
enum | _ERepresentation |
enum | _EEndianess |
enum | _ENameSpace |
enum | _EStandardNameSpace |
enum | _EYesNo |
typedef CPointer< IBase > | CBasePtr SmartPointer for IBase interface pointer. |
typedef CPointer< INode > | CNodePtr SmartPointer for INode interface pointer. |
typedef CPointer< IValue > | CValuePtr SmartPointer for IValue interface pointer. |
typedef CPointer< ICategory > | CCategoryPtr SmartPointer for ICategory interface pointer. |
typedef CPointer< IBoolean > | CBooleanPtr SmartPointer for IBoolean interface pointer. |
typedef CPointer< IInteger > | CIntegerPtr SmartPointer for IInteger interface pointer. |
typedef CPointer< IString > | CStringPtr SmartPointer for IString interface pointer. |
typedef CPointer< IRegister > | CRegisterPtr SmartPointer for IRegister interface pointer. |
typedef CPointer< IEnumeration > | CEnumerationPtr SmartPointer for IEnumeration interface pointer. |
typedef CPointer< IEnumEntry > | CEnumEntryPtr SmartPointer for IEnumEntry interface pointer. |
typedef CPointer< IPort > | CPortPtr SmartPointer for IPort interface pointer. |
typedef CPointer< IPortReplay > | CPortReplayPtr SmartPointer for IPortReplay interface pointer. |
typedef CPointer< IPortRecorder > | CPortRecorderPtr SmartPointer for IPortRecorder interface pointer. |
typedef CPointer< IPortWriteList, IPortWriteList > | CPortWriteListPtr SmartPointer for IPortWriteList interface pointer. |
typedef CPointer< IChunkPort > | CChunkPortPtr SmartPointer for IChunkPort interface pointer. |
typedef CPointer< INodeMap, INodeMap > | CNodeMapPtr SmartPointer for INodeMap interface pointer. |
typedef CPointer< IDeviceInfo, INodeMap > | CDeviceInfoPtr SmartPointer for IDeviceInfo interface pointer. |
typedef CPointer< IUserData, INodeMap > | CNodeMapUserDataPtr SmartPointer for IUserData interface pointer. |
typedef CPointer< IUserData > | CNodeUserDataPtr SmartPointer for IUserData interface pointer. |
typedef CPointer< ISelector > | CSelectorPtr SmartPointer for ISelector interface pointer. |
typedef CPointer< ICommand > | CCommandPtr SmartPointer for ICommand interface pointer. |
typedef enum GenApi::_ESign | ESign |
typedef enum GenApi::_EAccessMode | EAccessMode |
typedef enum GenApi::_EVisibility | EVisibility |
typedef enum GenApi::_ECachingMode | ECachingMode |
typedef enum GenApi::_ERepresentation | ERepresentation |
typedef enum GenApi::_EEndianess | EEndianess |
typedef enum GenApi::_ENameSpace | ENameSpace |
typedef enum GenApi::_EStandardNameSpace | EStandardNameSpace |
typedef enum GenApi::_EYesNo | EYesNo |
Functions#
名前 | |
---|---|
template <class Function > intptr_t | Register(INode * pNode, Function f, ECallbackType CallbackType =cbPostInsideLock) Register a C-function as a callback. |
template <class Client ,class Member > intptr_t | Register(INode * pNode, Client & c, Member m, ECallbackType CallbackType =cbPostInsideLock) Register a C++-member function a callback. |
Types Documentation#
enum _ESign#
Enumerator | 値 | 説明 |
---|---|---|
Signed | Integer is signed. | |
Unsigned | Integer is unsigned. | |
_UndefinedSign | Object is not yet initialized. |
signed or unsigned integers
enum _EAccessMode#
Enumerator | 値 | 説明 |
---|---|---|
NI | Not implemented. | |
NA | Not available. | |
WO | Write Only. | |
RO | Read Only. | |
RW | Read and Write. | |
_UndefinedAccesMode | Object is not yet initialized. | |
_CycleDetectAccesMode | used internally for AccessMode cycle detection |
access mode of a node
enum _EVisibility#
Enumerator | 値 | 説明 |
---|---|---|
Beginner | 0 | Always visible. |
Expert | 1 | Visible for experts or Gurus. |
Guru | 2 | Visible for Gurus. |
Invisible | 3 | Not Visible. |
_UndefinedVisibility | 99 | Object is not yet initialized. |
recommended visibility of a node
enum _ECachingMode#
Enumerator | 値 | 説明 |
---|---|---|
NoCache | Do not use cache. | |
WriteThrough | Write to cache and register. | |
WriteAround | Write to register, write to cache on read. | |
_UndefinedCachingMode | Not yet initialized. |
caching mode of a register
enum _ERepresentation#
Enumerator | 値 | 説明 |
---|---|---|
Linear | Slider with linear behavior. | |
Logarithmic | Slider with logarithmic behaviour. | |
Boolean | Check box. | |
PureNumber | Decimal number in an edit control. | |
HexNumber | Hex number in an edit control. | |
IPV4Address | IP-Address. | |
MACAddress | MAC-Address. | |
_UndefinedRepresentation |
recommended representation of a node value
enum _EEndianess#
Enumerator | 値 | 説明 |
---|---|---|
BigEndian | Register is big endian. | |
LittleEndian | Register is little endian. | |
_UndefinedEndian | Object is not yet initialized. |
Endianess of a value in a register
enum _ENameSpace#
Enumerator | 値 | 説明 |
---|---|---|
Custom | name resides in custom namespace | |
Standard | name resides in one of the standard namespaces | |
_UndefinedNameSpace | Object is not yet initialized. |
Defines if a node name is standard or custom
enum _EStandardNameSpace#
Enumerator | 値 | 説明 |
---|---|---|
None | name resides in custom namespace | |
GEV | name resides in GigE Vision namespace | |
IIDC | name resides in 1394 IIDC namespace | |
CL | name resides in camera link namespace | |
USB | name resides in USB namespace | |
_UndefinedStandardNameSpace | Object is not yet initialized. |
Defines from which standard namespace a node name comes from
enum _EYesNo#
Enumerator | 値 | 説明 |
---|---|---|
はい | 1 | yes |
いいえ | 0 | no |
_UndefinedYesNo | 2 | Object is not yet initialized. |
Defines the choices of a Yes/No alternatives
typedef CBasePtr#
SmartPointer for IBase interface pointer.
typedef CNodePtr#
SmartPointer for INode interface pointer.
typedef CValuePtr#
SmartPointer for IValue interface pointer.
typedef CCategoryPtr#
SmartPointer for ICategory interface pointer.
typedef CBooleanPtr#
SmartPointer for IBoolean interface pointer.
typedef CIntegerPtr#
SmartPointer for IInteger interface pointer.
typedef CStringPtr#
SmartPointer for IString interface pointer.
typedef CRegisterPtr#
SmartPointer for IRegister interface pointer.
typedef CEnumerationPtr#
SmartPointer for IEnumeration interface pointer.
typedef CEnumEntryPtr#
SmartPointer for IEnumEntry interface pointer.
typedef CPortPtr#
SmartPointer for IPort interface pointer.
typedef CPortReplayPtr#
SmartPointer for IPortReplay interface pointer.
typedef CPortRecorderPtr#
SmartPointer for IPortRecorder interface pointer.
typedef CPortWriteListPtr#
SmartPointer for IPortWriteList interface pointer.
typedef CChunkPortPtr#
SmartPointer for IChunkPort interface pointer.
typedef CNodeMapPtr#
SmartPointer for INodeMap interface pointer.
typedef CDeviceInfoPtr#
SmartPointer for IDeviceInfo interface pointer.
typedef CNodeMapUserDataPtr#
SmartPointer for IUserData interface pointer.
typedef CNodeUserDataPtr#
SmartPointer for IUserData interface pointer.
typedef CSelectorPtr#
SmartPointer for ISelector interface pointer.
typedef CCommandPtr#
SmartPointer for ICommand interface pointer.
typedef ESign#
signed or unsigned integers
typedef EAccessMode#
access mode of a node
typedef EVisibility#
recommended visibility of a node
typedef ECachingMode#
caching mode of a register
typedef ERepresentation#
recommended representation of a node value
typedef EEndianess#
Endianess of a value in a register
typedef ENameSpace#
Defines if a node name is standard or custom
typedef EStandardNameSpace#
Defines from which standard namespace a node name comes from
typedef EYesNo#
Defines the choices of a Yes/No alternatives
Functions Documentation#
function Register#
template <class Function >
intptr_t Register(
INode * pNode,
Function f,
ECallbackType CallbackType =cbPostInsideLock
)
Register a C-function as a callback.
function Register#
template <class Client ,
class Member >
intptr_t Register(
INode * pNode,
Client & c,
Member m,
ECallbackType CallbackType =cbPostInsideLock
)
Register a C++-member function a callback.