PLCamera.TestPatternEnum Class#
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.TestPatternEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.TestPatternEnum | Initializes a new instance of the PLCamera.TestPatternEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Black | The camera generates a black test pattern. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
ColorDiagonalSawtooth8 | The camera generates a test image with a color diagonal sawtooth pattern. Applies to: dart USB and pulse USB | |
GreyDiagonalSawtooth8 | The camera generates a test image with a gray diagonal sawtooth pattern. Applies to: dart USB and pulse USB | |
名前 | The full name of TestPattern (Overrides ParameterListEnum.Name.) | |
Off | No test pattern is generated. The original image is displayed. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB | |
Testimage1 | The camera generates a test image with the test image 1 pattern. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB | |
Testimage2 | The camera generates a test image with the test image 2 pattern. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Testimage3 | The camera generates a test image with the test image 3 pattern. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Testimage6 | The camera generates a test image with the test image 6 pattern. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
White | The camera generates a white test pattern. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of TestPattern (Overrides Object.ToString()()()().) |
PLCamera.TestPatternEnum.ToString Method#
The full name of TestPattern
Return Value#
Type: String
Returns the full name of TestPattern
PLCamera.TestPatternEnum Constructor#
Initializes a new instance of the PLCamera.TestPatternEnum class
PLCamera.TestPatternEnum.Black Property#
The camera generates a black test pattern.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TestPatternEnum.ColorDiagonalSawtooth8 Property#
The camera generates a test image with a color diagonal sawtooth pattern.
Applies to: dart USB and pulse USB
PLCamera.TestPatternEnum.GreyDiagonalSawtooth8 Property#
The camera generates a test image with a gray diagonal sawtooth pattern.
Applies to: dart USB and pulse USB
PLCamera.TestPatternEnum.Name Property#
The full name of TestPattern
PLCamera.TestPatternEnum.Off Property#
No test pattern is generated. The original image is displayed.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.TestPatternEnum.Testimage1 Property#
The camera generates a test image with the test image 1 pattern.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB
PLCamera.TestPatternEnum.Testimage2 Property#
The camera generates a test image with the test image 2 pattern.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TestPatternEnum.Testimage3 Property#
The camera generates a test image with the test image 3 pattern.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TestPatternEnum.Testimage6 Property#
The camera generates a test image with the test image 6 pattern.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TestPatternEnum.White Property#
The camera generates a white test pattern.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB