ImageWindow Class#
Inheritance Hierarchy#
System.Object
Basler.Pylon.ImageWindow
Syntax#
C#
VB
The ImageWindow type exposes the following members.
Constructors#
名前 | 説明 | |
---|---|---|
ImageWindow | Initializes a new instance of the ImageWindow class |
方法#
名前 | 説明 | |
---|---|---|
Close | Closes and destroys a window opened by using DisplayImage. | |
DisplayImage(Int32, IImage) | Displays an image on screen. | |
DisplayImage(Int32, IntPtr, Int64, PixelType, Int32, Int32, Int32, ImageOrientation) | Displays the contents of a raw image buffer on screen. | |
DisplayImage(T)(Int32, T[], PixelType, Int32, Int32, Int32, ImageOrientation) | Displays the contents of an image buffer on screen. | |
Handle | Returns the window handle of the image window. | |
Hide | Hides the image window. | |
Show(Int32) | Shows the image window. | |
Show(Int32, ShowMode) | Shows or hides the image window. |
ImageWindow.Close Method#
Closes and destroys a window opened by using DisplayImage.
Syntax#
C#
VB
パラメーター#
- windowIndex
- Type: System.Int32
The index of the window to be closed. Valid window indexes range from 0 to 31.
Remarks#
Thread Safety:This method is thread-safe.
Error Safety: Does not throw exceptions.
ImageWindow.DisplayImage Method (Int32, IImage)#
Displays an image on screen.
Syntax#
C#
VB
パラメーター#
- windowIndex
- Type: System.Int32
The index of the image window. Valid window indexes range from 0 to 31. - image
- Type: Basler.Pylon.IImage
The image to display in the window.
Remarks#
This method displays the image or the grab result in a window. Using this method is the easiest way to display an image on screen.
You can pass any IImage-based object. If the window hasn't been created before, it will be created with default positions and the image will be shown. When the method returns, you may dispose the image.
If you pass an empty or invalid image (e.g., IImage.IsValid() returns false), the window will be cleared. To close the window call Close()
- The window specified by windowIndex will be created and shown on screen.
- If the image passed is valid, it is shown in the window specified by windowIndex.
- If the image passed is invalid, the window specified by windowIndex will be cleared.
Error Safety: Can throw an exception if the windowIndex passed is invalid or if the window could not be created.
ImageWindow.DisplayImage Method (Int32, IntPtr, Int64, PixelType, Int32, Int32, Int32, ImageOrientation)#
Displays the contents of a raw image buffer on screen.
Syntax#
C#
public static void DisplayImage(
int windowIndex,
IntPtr pBuffer,
long bufferSize,
PixelType pixelType,
int width,
int height,
int paddingX,
ImageOrientation orientation
)
VB
Public Shared Sub DisplayImage (
windowIndex As Integer,
pBuffer As IntPtr,
bufferSize As Long,
pixelType As PixelType,
width As Integer,
height As Integer,
paddingX As Integer,
orientation As ImageOrientation
)
パラメーター#
- windowIndex
- Type: System.Int32
The index of the image window. Valid window indexes range from 0 to 31. - pBuffer
- Type: System.IntPtr
Pointer to the buffer containing the image data. - bufferSize
- Type: System.Int64
Size of the buffer in bytes. - pixelType
- Type: Basler.Pylon.PixelType
The pixel type of the image data in the buffer. - width
- Type: System.Int32
The number of pixels in a row of the image data in the buffer. - height
- Type: System.Int32
The number of rows in the image data in the buffer. - paddingX
- Type: System.Int32
The number of extra data bytes at the end of each row. - orientation
- Type: Basler.Pylon.ImageOrientation
The vertical orientation of the image in the image buffer.
Remarks#
This method displays the contents of a raw buffer in a window.
If the window hasn't been created before, it will be created with default positions. When the method returns, you may free the image buffer.
If you pass an empty or invalid buffer (e.g., pBuffer or bufferSize are invalid), the window will be cleared. To close the window call Close(Int32).
- The window specified by windowIndex will be created and shown on screen.
- If the image passed is valid, it is shown in the window specified by windowIndex.
- If the image passed is invalid, the window specified by windowIndex will be cleared.
Error Safety: Can throw an exception if the windowIndex, width, height, or paddingX passed are invalid or if the window could not be created.
ImageWindow.DisplayImage(T) Method (Int32, T[], PixelType, Int32, Int32, Int32, ImageOrientation)#
Displays the contents of an image buffer on screen.
Syntax#
C#
public static void DisplayImage<T>(
int windowIndex,
T[] buffer,
PixelType pixelType,
int width,
int height,
int paddingX,
ImageOrientation orientation
)
VB
Public Shared Sub DisplayImage(Of T) (
windowIndex As Integer,
buffer As T(),
pixelType As PixelType,
width As Integer,
height As Integer,
paddingX As Integer,
orientation As ImageOrientation
)
パラメーター#
- windowIndex
- Type: System.Int32
The index of the image window. Valid window indexes range from 0 to 31. - buffer
- Type: T[]
The typed array containing the image data. - pixelType
- Type: Basler.Pylon.PixelType
The pixel type of the image data in the buffer. - width
- Type: System.Int32
The number of pixels in a row of the image data in the buffer. - height
- Type: System.Int32
The number of rows in the image data in the buffer. - paddingX
- Type: System.Int32
The number of extra data bytes at the end of each row. - orientation
- Type: Basler.Pylon.ImageOrientation
The vertical orientation of the image in the image buffer.
Type Parameters#
- T
- The value type of the buffer array containing the image data.
Remarks#
This method displays the contents of a buffer in a window.
If the window hasn't been created before, it will be created with default positions. When the method returns, you may free the image buffer.
If you pass an empty or invalid buffer (e.g., buffer is empty or invalid), the window will be cleared. To close the window call Close(Int32).
- The window specified by windowIndex will be created and shown on screen.
- If the image passed is valid, it is shown in the window specified by windowIndex.
- If the image passed is invalid, the window specified by windowIndex will be cleared.
Error Safety: Can throw an exception if the windowIndex, width, height, or paddingX passed are invalid or if the window could not be created.
ImageWindow.Handle Method#
Returns the window handle of the image window.
Syntax#
C#
VB
パラメーター#
- windowIndex
- Type: System.Int32
The index of the image window. Valid window indexes range from 0 to 31.
Return Value#
Type: IntPtr
Returns the native window handle (HWND) of the image window.
ImageWindow.Hide Method#
Hides the image window.
Syntax#
C#
VB
パラメーター#
- windowIndex
- Type: System.Int32
The index of the image window. Valid window indexes range from 0 to 31.
ImageWindow.Show Method (Int32)#
Shows the image window.
Syntax#
C#
VB
パラメーター#
- windowIndex
- Type: System.Int32
The index of the image window. Valid window indexes range from 0 to 31.
ImageWindow.Show Method (Int32, ShowMode)#
Shows or hides the image window.
Syntax#
C#
VB
パラメーター#
- windowIndex
- Type: System.Int32
The index of the image window. Valid window indexes range from 0 to 31. - showMode
- Type: Basler.Pylon.ShowMode
The mode. See the ShowMode enum class for details.
Remarks#
After you create a window using Create(), it will be invisible. You must call Show() to make the window visible.
ImageWindow Constructor#
Initializes a new instance of the ImageWindow class
Syntax#
C#
VB
ImageWindow.DisplayImage Method#
Overload List#
名前 | 説明 | |
---|---|---|
DisplayImage(Int32, IImage) | Displays an image on screen. | |
DisplayImage(T)(Int32, T[], PixelType, Int32, Int32, Int32, ImageOrientation) | Displays the contents of an image buffer on screen. | |
DisplayImage(Int32, IntPtr, Int64, PixelType, Int32, Int32, Int32, ImageOrientation) | Displays the contents of a raw image buffer on screen. |
ImageWindow.Show Method#
Overload List#
名前 | 説明 | |
---|---|---|
Show(Int32) | Shows the image window. | |
Show(Int32, ShowMode) | Shows or hides the image window. |