PLCamera.BslLightControlErrorStatusEnum Class#
Applies to: GigE and ace USB
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslLightControlErrorStatusEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslLightControlErrorStatusEnum | Initializes a new instance of the PLCamera.BslLightControlErrorStatusEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Device1 | Light device 1 is experiencing problems. For more information, select the device using the Light Device Selector parameter and then check the Light Device Last Error parameter. Applies to: GigE and ace USB | |
Device2 | Light device 2 is experiencing problems. For more information, select the device using the Light Device Selector parameter and then check the Light Device Last Error parameter. Applies to: GigE and ace USB | |
Device3 | Light device 3 is experiencing problems. For more information, select the device using the Light Device Selector parameter and then check the Light Device Last Error parameter. Applies to: GigE and ace USB | |
Device4 | Light device 4 is experiencing problems. For more information, select the device using the Light Device Selector parameter and then check the Light Device Last Error parameter. Applies to: GigE and ace USB | |
MultipleDevices | Multiple light devices are experiencing problems. For more information, select one device after the other using the Light Device Selector parameter and check the Light Device Last Error parameter to find out which devices are experiencing problems. Applies to: GigE and ace USB | |
名前 | The full name of BslLightControlErrorStatus (Overrides ParameterListEnum.Name.) | |
NoError | エラーは検出されませんでした。 Applies to: GigE and ace USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslLightControlErrorStatus (Overrides Object.ToString()()()().) |
PLCamera.BslLightControlErrorStatusEnum.ToString Method#
The full name of BslLightControlErrorStatus
Return Value#
Type: String
Returns the full name of BslLightControlErrorStatus
PLCamera.BslLightControlErrorStatusEnum Constructor#
Initializes a new instance of the PLCamera.BslLightControlErrorStatusEnum class
PLCamera.BslLightControlErrorStatusEnum.Device1 Property#
Light device 1 is experiencing problems. For more information, select the device using the Light Device Selector parameter and then check the Light Device Last Error parameter.
Applies to: GigE and ace USB
PLCamera.BslLightControlErrorStatusEnum.Device2 Property#
Light device 2 is experiencing problems. For more information, select the device using the Light Device Selector parameter and then check the Light Device Last Error parameter.
Applies to: GigE and ace USB
PLCamera.BslLightControlErrorStatusEnum.Device3 Property#
Light device 3 is experiencing problems. For more information, select the device using the Light Device Selector parameter and then check the Light Device Last Error parameter.
Applies to: GigE and ace USB
PLCamera.BslLightControlErrorStatusEnum.Device4 Property#
Light device 4 is experiencing problems. For more information, select the device using the Light Device Selector parameter and then check the Light Device Last Error parameter.
Applies to: GigE and ace USB
PLCamera.BslLightControlErrorStatusEnum.MultipleDevices Property#
Multiple light devices are experiencing problems. For more information, select one device after the other using the Light Device Selector parameter and check the Light Device Last Error parameter to find out which devices are experiencing problems.
Applies to: GigE and ace USB
PLCamera.BslLightControlErrorStatusEnum.Name Property#
The full name of BslLightControlErrorStatus
PLCamera.BslLightControlErrorStatusEnum.NoError Property#
エラーは検出されませんでした。
Applies to: GigE and ace USB