PLCamera.BslSerialBaudRateEnum Class#
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslSerialBaudRateEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslSerialBaudRateEnum | Initializes a new instance of the PLCamera.BslSerialBaudRateEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Baud115200 | A symbol rate of 115200 baud is used in serial communication. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Baud1200 | A symbol rate of 1200 baud is used in serial communication. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Baud19200 | A symbol rate of 19200 baud is used in serial communication. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Baud2400 | A symbol rate of 2400 baud is used in serial communication. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Baud38400 | A symbol rate of 38400 baud is used in serial communication. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Baud4800 | A symbol rate of 4800 baud is used in serial communication. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Baud57600 | A symbol rate of 57600 baud is used in serial communication. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
Baud9600 | A symbol rate of 9600 baud is used in serial communication. Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress | |
名前 | The full name of BslSerialBaudRate (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslSerialBaudRate (Overrides Object.ToString()()()().) |
PLCamera.BslSerialBaudRateEnum.ToString Method#
The full name of BslSerialBaudRate
Return Value#
Type: String
Returns the full name of BslSerialBaudRate
PLCamera.BslSerialBaudRateEnum Constructor#
Initializes a new instance of the PLCamera.BslSerialBaudRateEnum class
PLCamera.BslSerialBaudRateEnum.Baud115200 Property#
A symbol rate of 115200 baud is used in serial communication.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslSerialBaudRateEnum.Baud1200 Property#
A symbol rate of 1200 baud is used in serial communication.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslSerialBaudRateEnum.Baud19200 Property#
A symbol rate of 19200 baud is used in serial communication.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslSerialBaudRateEnum.Baud2400 Property#
A symbol rate of 2400 baud is used in serial communication.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslSerialBaudRateEnum.Baud38400 Property#
A symbol rate of 38400 baud is used in serial communication.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslSerialBaudRateEnum.Baud4800 Property#
A symbol rate of 4800 baud is used in serial communication.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslSerialBaudRateEnum.Baud57600 Property#
A symbol rate of 57600 baud is used in serial communication.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslSerialBaudRateEnum.Baud9600 Property#
A symbol rate of 9600 baud is used in serial communication.
Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslSerialBaudRateEnum.Name Property#
The full name of BslSerialBaudRate