PLTransportLayer.TriggerOutStatisticsSourceEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.TriggerOutStatisticsSourceEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLTransportLayer.TriggerOutStatisticsSourceEnum | Initializes a new instance of the PLTransportLayer.TriggerOutStatisticsSourceEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of TriggerOutStatisticsSource (Overrides ParameterListEnum.Name.) | |
PulseGenerator0 | The source for the output statistics is set to Pulse Generator 0. Applies to: CoaXPress | |
PulseGenerator1 | The source for the output statistics is set to Pulse Generator 1. Applies to: CoaXPress | |
PulseGenerator2 | The source for the output statistics is set to Pulse Generator 2. Applies to: CoaXPress | |
PulseGenerator3 | The source for the output statistics is set to Pulse Generator 3. Applies to: CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of TriggerOutStatisticsSource (Overrides Object.ToString()()()().) |
PLTransportLayer.TriggerOutStatisticsSourceEnum.ToString Method#
The full name of TriggerOutStatisticsSource
Return Value#
Type: String
Returns the full name of TriggerOutStatisticsSource
PLTransportLayer.TriggerOutStatisticsSourceEnum Constructor#
Initializes a new instance of the PLTransportLayer.TriggerOutStatisticsSourceEnum class
PLTransportLayer.TriggerOutStatisticsSourceEnum.Name Property#
The full name of TriggerOutStatisticsSource
PLTransportLayer.TriggerOutStatisticsSourceEnum.PulseGenerator0 Property#
The source for the output statistics is set to Pulse Generator 0.
Applies to: CoaXPress
PLTransportLayer.TriggerOutStatisticsSourceEnum.PulseGenerator1 Property#
The source for the output statistics is set to Pulse Generator 1.
Applies to: CoaXPress
PLTransportLayer.TriggerOutStatisticsSourceEnum.PulseGenerator2 Property#
The source for the output statistics is set to Pulse Generator 2.
Applies to: CoaXPress
PLTransportLayer.TriggerOutStatisticsSourceEnum.PulseGenerator3 Property#
The source for the output statistics is set to Pulse Generator 3.
Applies to: CoaXPress