PLCamera.BslLightSourcePresetEnum Class#
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslLightSourcePresetEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslLightSourcePresetEnum | Initializes a new instance of the PLCamera.BslLightSourcePresetEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Daylight5000K | The light source preset for image acquisitions with daylight of 5000 K is selected. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Daylight6500K | The light source preset for image acquisitions with daylight of 6500 K is selected. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
FactoryLED6000K | The light source preset for image acquisitions with LED light is selected. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
名前 | The full name of BslLightSourcePreset (Overrides ParameterListEnum.Name.) | |
Off | No light source preset is selected. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Tungsten | The light source preset for image acquisitions with tungsten incandescent light is selected. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslLightSourcePreset (Overrides Object.ToString()()()().) |
PLCamera.BslLightSourcePresetEnum.ToString Method#
The full name of BslLightSourcePreset
Return Value#
Type: String
Returns the full name of BslLightSourcePreset
PLCamera.BslLightSourcePresetEnum Constructor#
Initializes a new instance of the PLCamera.BslLightSourcePresetEnum class
PLCamera.BslLightSourcePresetEnum.Daylight5000K Property#
The light source preset for image acquisitions with daylight of 5000 K is selected.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.BslLightSourcePresetEnum.Daylight6500K Property#
The light source preset for image acquisitions with daylight of 6500 K is selected.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.BslLightSourcePresetEnum.FactoryLED6000K Property#
The light source preset for image acquisitions with LED light is selected.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.BslLightSourcePresetEnum.Name Property#
The full name of BslLightSourcePreset
PLCamera.BslLightSourcePresetEnum.Off Property#
No light source preset is selected.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.BslLightSourcePresetEnum.Tungsten Property#
The light source preset for image acquisitions with tungsten incandescent light is selected.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB