Basler _UniversalStreamParams#
クラス#
名前 | |
---|---|
class | Basler_UniversalStreamParams::CUniversalStreamParams_Params A parameter class containing all parameters as members that are available for pylon stream grabbers. |
class | Basler_UniversalStreamParams::CUniversalStreamParams_Params_v7_4_0 A parameter class containing all parameters as members that are available for pylon stream grabbers. |
タイプ#
名前 | |
---|---|
enum | AccessModeEnums { AccessMode_Control, AccessMode_Exclusive, AccessMode_Monitor, AccessMode_NotInitialized} Valid values for AccessMode. |
enum | StatusEnums { Status_Closed, Status_Locked, Status_NotInitialized, Status_Open} Valid values for Status. |
enum | StreamBufferHandlingModeEnums { StreamBufferHandlingMode_NewestOnly, StreamBufferHandlingMode_OldestFirst, StreamBufferHandlingMode_OldestFirstOverwrite} Valid values for StreamBufferHandlingMode. |
enum | StreamTypeEnums { StreamType_CL, StreamType_CLHS, StreamType_CXP, StreamType_CameraLink, StreamType_CameraLinkHS, StreamType_CoaXPress, StreamType_Custom, StreamType_GEV, StreamType_GigEVision, StreamType_Mixed, StreamType_U3V, StreamType_USB3Vision} Valid values for StreamType. |
enum | TransmissionTypeEnums { TransmissionType_LimitedBroadcast, TransmissionType_Multicast, TransmissionType_SubnetDirectedBroadcast, TransmissionType_Unicast, TransmissionType_UseCameraConfig} Valid values for TransmissionType. |
enum | TypeEnums { Type_NoDriverAvailable, Type_SocketDriver, Type_WindowsFilterDriver, Type_WindowsIntelPerformanceDriver} Valid values for Type. |
Types Documentation#
enum AccessModeEnums#
Enumerator | 値 | 説明 |
---|---|---|
AccessMode_Control | The application has control access to the device - Applies to: GigE and blaze. | |
AccessMode_Exclusive | The application has exclusive access to the device - Applies to: GigE and blaze. | |
AccessMode_Monitor | The application has monitoring, i e , read-only, access to the device - Applies to: GigE and blaze. | |
AccessMode_NotInitialized | Access to the device has not been initialized - Applies to: GigE and blaze. |
enum StatusEnums#
Enumerator | 値 | 説明 |
---|---|---|
Status_Closed | The stream grabber is closed - Applies to: GigE. | |
Status_Locked | The stream grabber is locked - Applies to: GigE. | |
Status_NotInitialized | The stream grabber is not initialized - Applies to: GigE. | |
Status_Open | The stream grabber is open - Applies to: GigE. |
Valid values for Status.
enum StreamBufferHandlingModeEnums#
Enumerator | 値 | 説明 |
---|---|---|
StreamBufferHandlingMode_NewestOnly | The application always gets the latest completed buffer (i e , the newest) - Applies to: CoaXPress and blaze. | |
StreamBufferHandlingMode_OldestFirst | The application always gets the buffer from the head of the output buffer queue (i e , the oldest available) - Applies to: CoaXPress and blaze. | |
StreamBufferHandlingMode_OldestFirstOverwrite | The application always gets the buffer from the head of the output buffer queue (i e , the oldest available) - Applies to: CoaXPress and blaze. |
Valid values for StreamBufferHandlingMode.
enum StreamTypeEnums#
Enumerator | 値 | 説明 |
---|---|---|
StreamType_CL | The data stream uses the Camera Link transport layer - Applies to: CoaXPress. | |
StreamType_CLHS | The data stream uses the Camera Link HS transport layer - Applies to: CoaXPress. | |
StreamType_CXP | The data stream uses the CoaXPress transport layer - Applies to: CoaXPress. | |
StreamType_CameraLink | Camera Link - Applies to: CoaXPress. | |
StreamType_CameraLinkHS | Camera Link High Speed - Applies to: CoaXPress. | |
StreamType_CoaXPress | CoaXPress - Applies to: CoaXPress. | |
StreamType_Custom | The data stream uses a custom transport layer - Applies to: CoaXPress. | |
StreamType_GEV | The data stream uses the GigE Vision transport layer - Applies to: CoaXPress. | |
StreamType_GigEVision | GigE Vision - Applies to: CoaXPress. | |
StreamType_Mixed | Different interface modules of the GenTL Producer are of different types - Applies to: CoaXPress. | |
StreamType_U3V | The data stream uses the USB3 Vision transport layer - Applies to: CoaXPress. | |
StreamType_USB3Vision | USB3 Vision - Applies to: CoaXPress. |
Valid values for StreamType.
enum TransmissionTypeEnums#
Enumerator | 値 | 説明 |
---|---|---|
TransmissionType_LimitedBroadcast | The stream data is sent to all devices in the local area network (255 255 255 255) - Applies to: GigE. | |
TransmissionType_Multicast | The stream data is sent to selected devices in the local network � - Applies to: GigE. | |
TransmissionType_SubnetDirectedBroadcast | The stream data is sent to all devices in the same subnet as the camera - Applies to: GigE. | |
TransmissionType_Unicast | The stream data is sent to a single device in the local network - Applies to: GigE and blaze. | |
TransmissionType_UseCameraConfig | The stream transmission configuration is read from the camera - Applies to: GigE and blaze. |
Valid values for TransmissionType.
enum TypeEnums#
Enumerator | 値 | 説明 |
---|---|---|
Type_NoDriverAvailable | No suitable driver is installed - Applies to: GigE and blaze. | |
Type_SocketDriver | The socket driver is used - Applies to: GigE and blaze. | |
Type_WindowsFilterDriver | The pylon GigE Vision Filter Driver is used - Applies to: GigE and blaze. | |
Type_WindowsIntelPerformanceDriver | The pylon GigE Vision Performance Driver is used - Applies to: GigE and blaze. |
Valid values for Type.