PLCamera.ROIZoneSelectorEnum Class#
Applies to: GigE and ace USB
Visibility: Expert
Selecting Parameters: ROIZoneMode, ROIZoneOffset, ROIZoneSize
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ROIZoneSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.ROIZoneSelectorEnum | Initializes a new instance of the PLCamera.ROIZoneSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of ROIZoneSelector (Overrides ParameterListEnum.Name.) | |
Zone0 | ROI zone 0 can be configured. Applies to: GigE and ace USB | |
Zone1 | ROI zone 1 can be configured. Applies to: GigE and ace USB | |
Zone2 | ROI zone 2 can be configured. Applies to: GigE and ace USB | |
Zone3 | ROI zone 3 can be configured. Applies to: GigE and ace USB | |
Zone4 | ROI zone 4 can be configured. Applies to: GigE and ace USB | |
Zone5 | ROI zone 5 can be configured. Applies to: GigE and ace USB | |
Zone6 | ROI zone 6 can be configured. Applies to: GigE and ace USB | |
Zone7 | ROI zone 7 can be configured. Applies to: GigE and ace USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of ROIZoneSelector (Overrides Object.ToString()()()().) |
PLCamera.ROIZoneSelectorEnum.ToString Method#
The full name of ROIZoneSelector
Return Value#
Type: String
Returns the full name of ROIZoneSelector
PLCamera.ROIZoneSelectorEnum Constructor#
Initializes a new instance of the PLCamera.ROIZoneSelectorEnum class
PLCamera.ROIZoneSelectorEnum.Name Property#
The full name of ROIZoneSelector
PLCamera.ROIZoneSelectorEnum.Zone0 Property#
ROI zone 0 can be configured.
Applies to: GigE and ace USB
PLCamera.ROIZoneSelectorEnum.Zone1 Property#
ROI zone 1 can be configured.
Applies to: GigE and ace USB
PLCamera.ROIZoneSelectorEnum.Zone2 Property#
ROI zone 2 can be configured.
Applies to: GigE and ace USB
PLCamera.ROIZoneSelectorEnum.Zone3 Property#
ROI zone 3 can be configured.
Applies to: GigE and ace USB
PLCamera.ROIZoneSelectorEnum.Zone4 Property#
ROI zone 4 can be configured.
Applies to: GigE and ace USB
PLCamera.ROIZoneSelectorEnum.Zone5 Property#
ROI zone 5 can be configured.
Applies to: GigE and ace USB
PLCamera.ROIZoneSelectorEnum.Zone6 Property#
ROI zone 6 can be configured.
Applies to: GigE and ace USB
PLCamera.ROIZoneSelectorEnum.Zone7 Property#
ROI zone 7 can be configured.
Applies to: GigE and ace USB