PLCamera.LegacyBinningVerticalEnum Class#
Applies to: CameraLink and GigE
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.LegacyBinningVerticalEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.LegacyBinningVerticalEnum | Initializes a new instance of the PLCamera.LegacyBinningVerticalEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of LegacyBinningVertical (Overrides ParameterListEnum.Name.) | |
Off | Vertical binning is disabled. Applies to: CameraLink and GigE | |
Two_Rows | Vertical binning is set to 2 rows. Applies to: CameraLink and GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of LegacyBinningVertical (Overrides Object.ToString()()()().) |
PLCamera.LegacyBinningVerticalEnum.ToString Method#
The full name of LegacyBinningVertical
Return Value#
Type: String
Returns the full name of LegacyBinningVertical
PLCamera.LegacyBinningVerticalEnum Constructor#
Initializes a new instance of the PLCamera.LegacyBinningVerticalEnum class
PLCamera.LegacyBinningVerticalEnum.Name Property#
The full name of LegacyBinningVertical
PLCamera.LegacyBinningVerticalEnum.Off Property#
Vertical binning is disabled.
Applies to: CameraLink and GigE
PLCamera.LegacyBinningVerticalEnum.Two_Rows Property#
Vertical binning is set to 2 rows.
Applies to: CameraLink and GigE