PLCamera.ExposureAutoEnum Class#
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ExposureAutoEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.ExposureAutoEnum | Initializes a new instance of the PLCamera.ExposureAutoEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Continuous | The exposure time is adjusted continuously while images are being acquired. The adjustment process will continue until the parameter is set to Once or Off. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB | |
名前 | The full name of ExposureAuto (Overrides ParameterListEnum.Name.) | |
Off | Automatic exposure time adjustment is disabled. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB | |
Once | The exposure time is adjusted automatically to reach the specified target value. When the target value has been reached, the auto function will automatically be set to Off and the new parameter value will be applied to the following images. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of ExposureAuto (Overrides Object.ToString()()()().) |
PLCamera.ExposureAutoEnum.ToString Method#
The full name of ExposureAuto
Return Value#
Type: String
Returns the full name of ExposureAuto
PLCamera.ExposureAutoEnum Constructor#
Initializes a new instance of the PLCamera.ExposureAutoEnum class
PLCamera.ExposureAutoEnum.Continuous Property#
The exposure time is adjusted continuously while images are being acquired. The adjustment process will continue until the parameter is set to Once or Off.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.ExposureAutoEnum.Name Property#
The full name of ExposureAuto
PLCamera.ExposureAutoEnum.Off Property#
Automatic exposure time adjustment is disabled.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.ExposureAutoEnum.Once Property#
The exposure time is adjusted automatically to reach the specified target value. When the target value has been reached, the auto function will automatically be set to Off and the new parameter value will be applied to the following images.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB