IRawParameter Interface#
Syntax#
C#
VB
The IRawParameter type exposes the following members.
プロパティ#
名前 | 説明 | |
---|---|---|
Advanced | The advanced parameter settings, if available. (Inherited from IParameter.) | |
FullName | The full name of the parameter including path information. (Inherited from IParameter.) | |
IsEmpty | Indicates if the parameter is empty. If true, the parameter is invalid or does not exist. If a requested parameter does not exist in a parameter collection, an empty parameter object will be returned to simplify handling. An empty parameter is never readable or writable. (Inherited from IParameter.) | |
IsReadable | Indicates if the parameter is readable. (Inherited from IParameter.) | |
IsWritable | Indicates if the parameter is writable. (Inherited from IParameter.) | |
名前 | The name of the parameter without path information. (Inherited from IParameter.) |
方法#
名前 | 説明 | |
---|---|---|
ParseAndSetValue | Parses the value as string and sets the value. (Inherited from IParameter.) | |
ReadRaw(Int64, IntPtr, Int64) | Reads raw data from the specified address into the buffer passed. | |
ReadRaw(T)(Int64, T[], Int32, Int32) | Reads raw data from the specified address into the array passed. | |
ToString | The parameter value as a string. (Inherited from IParameter.) | |
WriteRaw(Int64, IntPtr, Int64) | Writes raw data from the buffer passed to the specified address. | |
WriteRaw(T)(Int64, T[], Int32, Int32) | Writes raw data from the array passed to the specified address. |
Events#
名前 | 説明 | |
---|---|---|
ParameterChanged | This event fires after any of the parameter properties (value, readability, writability, or advanced parameter settings) have changed. (Inherited from IParameter.) | |
ParameterValueChanged | This event fires after the parameter value has changed. (Inherited from IParameter.) |
IRawParameter.ReadRaw Method (Int64, IntPtr, Int64)#
Reads raw data from the specified address into the buffer passed.
Syntax#
C#
VB
パラメーター#
- address
- Type: System.Int64
Starting address to read bufferSize number of bytes from. - pBuffer
- Type: System.IntPtr
The memory pointer to store the data read. - bufferSize
- Type: System.Int64
The number of bytes to read.
Remarks#
Some cameras may not report a failure if an error occurs and return 0 data instead.
Thread Safety: This method is synchronized with the source of the parameter collection, if any.
Error Safety: Can throw exceptions if reading fails or if the pointer is invalid.
IRawParameter.ReadRaw(T) Method (Int64, T[], Int32, Int32)#
Reads raw data from the specified address into the array passed.
Syntax#
C#
VB
Sub ReadRaw(Of T) (
address As Long,
ByRef buffer As T(),
startIndex As Integer,
length As Integer
)
パラメーター#
- address
- Type: System.Int64
Starting address to read bufferSize number of bytes from. - buffer
- Type: T[]
The one-dimensional array to store the data read. - startIndex
- Type: System.Int32
The zero-based index in the destination array where the data will be stored. - length
- Type: System.Int32
The number of array elements to store in the array.
Type Parameters#
- T
- The value type of the one-dimensional array to store the read data.
Remarks#
Some cameras may not report a failure if an error occurs and return 0 data instead.
The number of bytes read is determined by the length parameter and the size of an element in the array.
Preconditions:
- The array must be one-dimensional and elements must be of simple types.
Error Safety: Can throw exceptions if reading fails or if the array is not initialized.
IRawParameter.WriteRaw Method (Int64, IntPtr, Int64)#
Writes raw data from the buffer passed to the specified address.
Syntax#
C#
VB
パラメーター#
- address
- Type: System.Int64
Starting address to write bufferSize number of bytes to. - pBuffer
- Type: System.IntPtr
The memory pointer to read the data from. - bufferSize
- Type: System.Int64
The number of bytes to read from the buffer and write to the address.
Remarks#
Thread Safety: This method is synchronized with the source of the parameter collection, if any.
Error Safety: Can throw exceptions if writing fails or if the pointer is invalid.
IRawParameter.WriteRaw(T) Method (Int64, T[], Int32, Int32)#
Writes raw data from the array passed to the specified address.
Syntax#
C#
VB
パラメーター#
- address
- Type: System.Int64
Starting address to write bufferSize number of bytes to. - buffer
- Type: T[]
The one-dimensional array containing the data to store. - startIndex
- Type: System.Int32
The zero-based index in the array where writing data starts. - length
- Type: System.Int32
The number of array elements to write.
Type Parameters#
- T
- The value type of the one-dimensional array containing the data to store.
Remarks#
The number of bytes written is determined by the length parameter and the size of an element in the array.
Preconditions:
- The array must be one-dimensional and elements must be of simple types.
Error Safety: Can throw exceptions if writing fails or if the array is not initialized
IRawParameter.ReadRaw Method#
Overload List#
名前 | 説明 | |
---|---|---|
ReadRaw(Int64, IntPtr, Int64) | Reads raw data from the specified address into the buffer passed. | |
ReadRaw(T)(Int64, T[], Int32, Int32) | Reads raw data from the specified address into the array passed. |
IRawParameter.WriteRaw Method#
Overload List#
名前 | 説明 | |
---|---|---|
WriteRaw(Int64, IntPtr, Int64) | Writes raw data from the buffer passed to the specified address. | |
WriteRaw(T)(Int64, T[], Int32, Int32) | Writes raw data from the array passed to the specified address. |