PLInterface.InterfaceAppletEnum Class#
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLInterface.InterfaceAppletEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLInterface.InterfaceAppletEnum | Initializes a new instance of the PLInterface.InterfaceAppletEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Acq_DualCXP12Area | The Acq_DualCXP12Area applet is used to initialize the interface. Applies to: CoaXPress | |
Acq_DualCXP12Line | Applies to: CoaXPress | |
Acq_QuadCXP12Area | The Acq_QuadCXP12Area applet is used to initialize the interface. Applies to: CoaXPress | |
Acq_QuadCXP12Line | Applies to: CoaXPress | |
Acq_SingleCXP12Area | The Acq_SingleCXP12Area applet is used to initialize the interface. Applies to: CoaXPress | |
Acq_SingleCXP12Line | Applies to: CoaXPress | |
Acq_SingleCXP12x1Area | The Acq_SingleCXP12x1Area applet is used to initialize the interface. Applies to: CoaXPress | |
Acq_SingleCXP12x1Area_01 | The Acq_SingleCXP12x1Area_01 applet is used to initialize the interface. Applies to: CoaXPress | |
Acq_SingleCXP12x1Area_02 | The Acq_SingleCXP12x1Area_02 applet is used to initialize the interface. Applies to: CoaXPress | |
Acq_TripleCXP12Area | The Acq_TripleCXP12Area applet is used to initialize the interface. Applies to: CoaXPress | |
Acq_TripleCXP12Line | Applies to: CoaXPress | |
FrameGrabberTest | Applies to: CoaXPress | |
名前 | The full name of InterfaceApplet (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of InterfaceApplet (Overrides Object.ToString()()()().) |
PLInterface.InterfaceAppletEnum.ToString Method#
The full name of InterfaceApplet
Return Value#
Type: String
Returns the full name of InterfaceApplet
PLInterface.InterfaceAppletEnum Constructor#
Initializes a new instance of the PLInterface.InterfaceAppletEnum class
PLInterface.InterfaceAppletEnum.Acq_DualCXP12Area Property#
The Acq_DualCXP12Area applet is used to initialize the interface.
Applies to: CoaXPress
PLInterface.InterfaceAppletEnum.Acq_DualCXP12Line Property#
Applies to: CoaXPress
PLInterface.InterfaceAppletEnum.Acq_QuadCXP12Area Property#
The Acq_QuadCXP12Area applet is used to initialize the interface.
Applies to: CoaXPress
PLInterface.InterfaceAppletEnum.Acq_QuadCXP12Line Property#
Applies to: CoaXPress
PLInterface.InterfaceAppletEnum.Acq_SingleCXP12Area Property#
The Acq_SingleCXP12Area applet is used to initialize the interface.
Applies to: CoaXPress
PLInterface.InterfaceAppletEnum.Acq_SingleCXP12Line Property#
Applies to: CoaXPress
PLInterface.InterfaceAppletEnum.Acq_SingleCXP12x1Area Property#
The Acq_SingleCXP12x1Area applet is used to initialize the interface.
Applies to: CoaXPress
PLInterface.InterfaceAppletEnum.Acq_SingleCXP12x1Area_01 Property#
The Acq_SingleCXP12x1Area_01 applet is used to initialize the interface.
Applies to: CoaXPress
PLInterface.InterfaceAppletEnum.Acq_SingleCXP12x1Area_02 Property#
The Acq_SingleCXP12x1Area_02 applet is used to initialize the interface.
Applies to: CoaXPress
PLInterface.InterfaceAppletEnum.Acq_TripleCXP12Area Property#
The Acq_TripleCXP12Area applet is used to initialize the interface.
Applies to: CoaXPress
PLInterface.InterfaceAppletEnum.Acq_TripleCXP12Line Property#
Applies to: CoaXPress
PLInterface.InterfaceAppletEnum.FrameGrabberTest Property#
Applies to: CoaXPress
PLInterface.InterfaceAppletEnum.Name Property#
The full name of InterfaceApplet