PLCamera.BslImmediateTriggerModeEnum Class#
Applies to: dart USB and pulse USB
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslImmediateTriggerModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslImmediateTriggerModeEnum | Initializes a new instance of the PLCamera.BslImmediateTriggerModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of BslImmediateTriggerMode (Overrides ParameterListEnum.Name.) | |
Off | The Immediate Trigger mode is disabled. This increases the exposure start delay, but changes to image parameters become effective immediately. Applies to: dart USB and pulse USB | |
その | The Immediate Trigger mode is enabled. This reduces the exposure start delay. Applies to: dart USB and pulse USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslImmediateTriggerMode (Overrides Object.ToString()()()().) |
PLCamera.BslImmediateTriggerModeEnum.ToString Method#
The full name of BslImmediateTriggerMode
Return Value#
Type: String
Returns the full name of BslImmediateTriggerMode
PLCamera.BslImmediateTriggerModeEnum Constructor#
Initializes a new instance of the PLCamera.BslImmediateTriggerModeEnum class
PLCamera.BslImmediateTriggerModeEnum.Name Property#
The full name of BslImmediateTriggerMode
PLCamera.BslImmediateTriggerModeEnum.Off Property#
The Immediate Trigger mode is disabled. This increases the exposure start delay, but changes to image parameters become effective immediately.
Applies to: dart USB and pulse USB
PLCamera.BslImmediateTriggerModeEnum.On Property#
The Immediate Trigger mode is enabled. This reduces the exposure start delay.
Applies to: dart USB and pulse USB