GrabStopEventArgs Class#
Inheritance Hierarchy#
System.Object
System.EventArgs
Basler.Pylon.GrabStopEventArgs
Syntax#
C#
VB
The GrabStopEventArgs type exposes the following members.
Constructors#
名前 | 説明 | |
---|---|---|
GrabStopEventArgs() | Creates an instance with the grab stop reason set to UserRequest and no error message. | |
GrabStopEventArgs(GrabStopReason, String) | Creates an instance with a specified grab stop reason and an error message. |
プロパティ#
名前 | 説明 | |
---|---|---|
ErrorMessage | The message that is displayed if the grab stopped because of an error. | |
Reason | The reason why the GrabStopping or GrabStopped event occurred. |
GrabStopEventArgs Constructor#
Creates an instance with the grab stop reason set to UserRequest and no error message.
Syntax#
C#
VB
GrabStopEventArgs Constructor (GrabStopReason, String)#
Creates an instance with a specified grab stop reason and an error message.
Syntax#
C#
VB
パラメーター#
- reason
- Type: Basler.Pylon.GrabStopReason
The reason why the grab stop event occurred. - errorMessage
- Type: System.String
The message that is displayed if the grab stopped because of an error.
GrabStopEventArgs Constructor#
Overload List#
名前 | 説明 | |
---|---|---|
GrabStopEventArgs() | Creates an instance with the grab stop reason set to UserRequest and no error message. | |
GrabStopEventArgs(GrabStopReason, String) | Creates an instance with a specified grab stop reason and an error message. |
GrabStopEventArgs.ErrorMessage Property#
The message that is displayed if the grab stopped because of an error.
Syntax#
C#
VB
Property Value#
Type: String
GrabStopEventArgs.Reason Property#
The reason why the GrabStopping or GrabStopped event occurred.
Syntax#
C#
VB
Property Value#
Type: GrabStopReason