IAdvancedParameterAccess Interface#
Syntax#
C#
VB
The IAdvancedParameterAccess type exposes the following members.
方法#
名前 | 説明 | |
---|---|---|
ContainsProperty | Returns true if the property key passed exists. | |
GetLock | Advanced: Returns the object used to lock access to the parameter. | |
GetProperty | Returns the value for the property specified by the key. | |
GetPropertyOrDefault | Gets the property value if the given property key exists. Otherwise, returns the default value. | |
更新 | Invalidates all cached values. | |
SetProperty | Sets the value for the property specified by the key. |
IAdvancedParameterAccess.ContainsProperty Method#
Returns true if the property key passed exists.
Syntax#
C#
VB
パラメーター#
- key
- Type: System.String
String containing the name of the property. You can use the AdvancedParameterAccessKey class to get a list of possible values.
Return Value#
Type: Boolean
Returns true if the property key passed exists.
Remarks#
Thread Safety:This method is synchronized with the source of the parameter collection, if any.
Error Safety:Does not throw exceptions.
IAdvancedParameterAccess.GetLock Method#
Advanced: Returns the object used to lock access to the parameter.
Syntax#
C#
VB
Return Value#
Type: Object
Returns the object used to lock access to the parameter. If there is no lock object a null reference will be returned.
Remarks#
Returns the object used to lock the access to the parameter. This is an advanced function.
For each successful acquisition of the lock you must release the lock. Failure to do so may result in lockups and indeterministic behaviour of pylon objects.
Thread Safety:This method is thread-safe.
Error Safety:Does not throw exceptions.
IAdvancedParameterAccess.GetProperty Method#
Returns the value for the property specified by the key.
Syntax#
C#
VB
パラメーター#
- key
- Type: System.String
String containing the name of the property. You can use the AdvancedParameterAccessKey class to get a list of possible values.
Return Value#
Type: String
Returns the string value for the property specified by the key.
Remarks#
Thread Safety:This method is synchronized with the source of the parameter collection, if any.
Error Safety: Can throw exceptions. Throws a System.ArgumentNullException if the key passed is null. Throws a System.NotSupportedException if the key passed is not supported.
IAdvancedParameterAccess.GetPropertyOrDefault Method#
Gets the property value if the given property key exists. Otherwise, returns the default value.
Syntax#
C#
VB
パラメーター#
- key
- Type: System.String
The key of the property to look up. The comparison is case sensitive. - defaultValue
- Type: System.String
The default value returned if the property key is not found.
Return Value#
Type: String
Returns the property value if the given property key exists. Otherwise, returns the default value.
Remarks#
Thread Safety:This method is synchronized with the source of the parameter collection, if any.
Error Safety: Can throw exceptions.
IAdvancedParameterAccess.Refresh Method#
Invalidates all cached values.
Syntax#
C#
VB
Remarks#
Some parameter values are cached, e.g. to minimize the overhead while communicating with a camera device. You can call this method to force an invalidation of the cached values. On the next read of the parameter, the value will be read from the source instead of returning a cached value. This will raise a ParameterChanged event. This method can be used to reread the value in the ParameterChanged event handler.
Thread Safety:This method is synchronized with the source of the parameter collection, if any.
Error Safety:Can throw exceptions. Parameter event handlers can throw exceptions.
IAdvancedParameterAccess.SetProperty Method#
Sets the value for the property specified by the key.
Syntax#
C#
VB
パラメーター#
- key
- Type: System.String
String containing the name of the property. You can use the AdvancedParameterAccessKey class to get a list of possible values. - value
- Type: System.String
String containing the value of the property to set.
Remarks#
Thread Safety:This method is synchronized with the source of the parameter collection, if any.
Error Safety: Can throw exceptions. Throws a System.ArgumentNullException if the key passed is null. Throws a System.NotSupportedException if writing the key passed is not supported.