PLTransportLayer.DeviceTypeEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.DeviceTypeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLTransportLayer.DeviceTypeEnum | Initializes a new instance of the PLTransportLayer.DeviceTypeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
CameraLink | Camera Link Applies to: CoaXPress | |
CameraLinkHS | Camera Link High Speed. Applies to: CoaXPress | |
CL | The device uses the Camera Link transport layer. Applies to: CoaXPress | |
CLHS | The device uses the Camera Link HS transport layer. Applies to: CoaXPress | |
CoaXPress | CoaXPress. Applies to: CoaXPress | |
Custom | The device uses a custom transport layer. Applies to: CoaXPress | |
CXP | The device uses the CoaXPress transport layer. Applies to: CoaXPress | |
GEV | The device uses the GigE Vision transport layer. Applies to: CoaXPress | |
GigEVision | GigE Vision Applies to: CoaXPress | |
Mixed | Different interface modules of the GenTL Producer are of different types. Applies to: CoaXPress | |
名前 | The full name of DeviceType (Overrides ParameterListEnum.Name.) | |
U3V | The device uses the USB3 Vision transport layer. Applies to: CoaXPress | |
USB3Vision | USB3 Vision. Applies to: CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of DeviceType (Overrides Object.ToString()()()().) |
PLTransportLayer.DeviceTypeEnum.ToString Method#
The full name of DeviceType
Return Value#
Type: String
Returns the full name of DeviceType
PLTransportLayer.DeviceTypeEnum Constructor#
Initializes a new instance of the PLTransportLayer.DeviceTypeEnum class
PLTransportLayer.DeviceTypeEnum.CameraLink Property#
Camera Link
Applies to: CoaXPress
PLTransportLayer.DeviceTypeEnum.CameraLinkHS Property#
Camera Link High Speed.
Applies to: CoaXPress
PLTransportLayer.DeviceTypeEnum.CL Property#
The device uses the Camera Link transport layer.
Applies to: CoaXPress
PLTransportLayer.DeviceTypeEnum.CLHS Property#
The device uses the Camera Link HS transport layer.
Applies to: CoaXPress
PLTransportLayer.DeviceTypeEnum.CoaXPress Property#
CoaXPress.
Applies to: CoaXPress
PLTransportLayer.DeviceTypeEnum.Custom Property#
The device uses a custom transport layer.
Applies to: CoaXPress
PLTransportLayer.DeviceTypeEnum.CXP Property#
The device uses the CoaXPress transport layer.
Applies to: CoaXPress
PLTransportLayer.DeviceTypeEnum.GEV Property#
The device uses the GigE Vision transport layer.
Applies to: CoaXPress
PLTransportLayer.DeviceTypeEnum.GigEVision Property#
GigE Vision
Applies to: CoaXPress
PLTransportLayer.DeviceTypeEnum.Mixed Property#
Different interface modules of the GenTL Producer are of different types.
Applies to: CoaXPress
PLTransportLayer.DeviceTypeEnum.Name Property#
The full name of DeviceType
PLTransportLayer.DeviceTypeEnum.U3V Property#
The device uses the USB3 Vision transport layer.
Applies to: CoaXPress
PLTransportLayer.DeviceTypeEnum.USB3Vision Property#
USB3 Vision.
Applies to: CoaXPress