PLCamera.ImageCompressionRateOptionEnum Class#
Applies to: ace 2 GigE and ace 2 USB
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ImageCompressionRateOptionEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.ImageCompressionRateOptionEnum | Initializes a new instance of the PLCamera.ImageCompressionRateOptionEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
FixRatio | The camera compresses acquired images. If lossless compression can't be achieved, image quality is reduced. Applies to: ace 2 GigE and ace 2 USB | |
Lossless | The camera uses lossless compression. This means that the restored image will be identical to the original image. Applies to: ace 2 GigE and ace 2 USB | |
名前 | The full name of ImageCompressionRateOption (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of ImageCompressionRateOption (Overrides Object.ToString()()()().) |
PLCamera.ImageCompressionRateOptionEnum.ToString Method#
The full name of ImageCompressionRateOption
Return Value#
Type: String
Returns the full name of ImageCompressionRateOption
PLCamera.ImageCompressionRateOptionEnum Constructor#
Initializes a new instance of the PLCamera.ImageCompressionRateOptionEnum class
PLCamera.ImageCompressionRateOptionEnum.FixRatio Property#
The camera compresses acquired images. If lossless compression can't be achieved, image quality is reduced.
Applies to: ace 2 GigE and ace 2 USB
PLCamera.ImageCompressionRateOptionEnum.Lossless Property#
The camera uses lossless compression. This means that the restored image will be identical to the original image.
Applies to: ace 2 GigE and ace 2 USB
PLCamera.ImageCompressionRateOptionEnum.Name Property#
The full name of ImageCompressionRateOption