IParameter Interface#
Syntax#
C#
VB
The IParameter type exposes the following members.
プロパティ#
名前 | 説明 | |
---|---|---|
Advanced | The advanced parameter settings, if available. | |
FullName | The full name of the parameter including path information. | |
IsEmpty | Indicates if the parameter is empty. If true, the parameter is invalid or does not exist. If a requested parameter does not exist in a parameter collection, an empty parameter object will be returned to simplify handling. An empty parameter is never readable or writable. | |
IsReadable | Indicates if the parameter is readable. | |
IsWritable | Indicates if the parameter is writable. | |
名前 | The name of the parameter without path information. |
方法#
名前 | 説明 | |
---|---|---|
ParseAndSetValue | Parses the value as string and sets the value. | |
ToString | The parameter value as a string. |
Events#
名前 | 説明 | |
---|---|---|
ParameterChanged | This event fires after any of the parameter properties (value, readability, writability, or advanced parameter settings) have changed. | |
ParameterValueChanged | This event fires after the parameter value has changed. |
IParameter.ParameterChanged Event#
This event fires after any of the parameter properties (value, readability, writability, or advanced parameter settings) have changed.
Syntax#
C#
VB
値#
Type: System.EventHandler(ParameterChangedEventArgs)
Remarks#
Thread Safety: The firing of the event is synchronized with the source of the parameter collection.
Error Safety: Exceptions from this event will propagate through. The notification of event handlers stops when an exception is triggered.
IParameter.ParameterValueChanged Event#
This event fires after the parameter value has changed.
Syntax#
C#
VB
値#
Type: System.EventHandler(ParameterValueChangedEventArgs)
Remarks#
Thread Safety: The firing of the event is synchronized with the source of the parameter collection.
Error Safety: Exceptions from this event will propagate through. The notification of event handlers stops when an exception is triggered.
IParameter.ParseAndSetValue Method#
Parses the value as string and sets the value.
Syntax#
C#
VB
パラメーター#
- value
- Type: System.String
The value as string.
Remarks#
Preconditions:
- The parameter must be writable.
- The value must be valid.
Error Safety: Can throw exceptions, e.g. if parsing or writing the value fails.
IParameter.ToString Method#
The parameter value as a string.
Syntax#
C#
VB
Return Value#
Type: String
Returns the parameter value as a string. If the value could not be read, one of the following strings are returned:
Remarks#
Thread Safety: This method is synchronized with the source of the parameter collection, if any.
Error Safety: Does not throw exceptions.
IParameter.Advanced Property#
The advanced parameter settings, if available.
Syntax#
C#
VB
Return Value#
Type: IAdvancedParameterAccess
Returns advanced parameter settings. Returns null if no advanced parameter settings are available.
Remarks#
Thread Safety: This method is synchronized with the source of the parameter collection, if any.
Error Safety: Does not throw exceptions.
IParameter.FullName Property#
The full name of the parameter including path information.
Syntax#
C#
VB
Return Value#
Type: String
Returns the full name of the parameter.
Remarks#
Thread Safety: This method is synchronized with the source of the parameter collection, if any.
Error Safety: Does not throw exceptions.
IParameter.IsEmpty Property#
Indicates if the parameter is empty. If true, the parameter is invalid or does not exist. If a requested parameter does not exist in a parameter collection, an empty parameter object will be returned to simplify handling. An empty parameter is never readable or writable.
Syntax#
C#
VB
Property Value#
Type: Boolean
Remarks#
Thread Safety:This method is synchronized with the source of the parameter collection, if any.
Error Safety:Does not throw exceptions.
IParameter.IsReadable Property#
Indicates if the parameter is readable.
Syntax#
C#
VB
Return Value#
Type: Boolean
Returns true if the parameter is readable.
Remarks#
Thread Safety: This method is synchronized with the source of the parameter collection, if any.
Error Safety: Does not throw exceptions.
IParameter.IsWritable Property#
Indicates if the parameter is writable.
Syntax#
C#
VB
Return Value#
Type: Boolean
Returns true if the parameter is writable.
Remarks#
Thread Safety: This method is synchronized with the source of the parameter collection, if any.
Error Safety: Does not throw exceptions.
IParameter.Name Property#
The name of the parameter without path information.
Syntax#
C#
VB
Return Value#
Type: String
Returns the name of the parameter without path information.
Remarks#
Thread Safety: This method is synchronized with the source of the parameter collection, if any.
Error Safety: Does not throw exceptions.