PLCamera.PtpClockAccuracyEnum Class#
Applies to: ace 2 GigE
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.PtpClockAccuracyEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.PtpClockAccuracyEnum | Initializes a new instance of the PLCamera.PtpClockAccuracyEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
GreaterThan10s | The expected accuracy of the PTP device clock is greater than 10 seconds. Applies to: ace 2 GigE | |
名前 | The full name of PtpClockAccuracy (Overrides ParameterListEnum.Name.) | |
Unknown | The expected accuracy of the PTP device clock is unknown. Applies to: ace 2 GigE | |
Within100ms | The expected accuracy of the PTP device clock is within 100 milliseconds. Applies to: ace 2 GigE | |
Within100ns | The expected accuracy of the PTP device clock is within 100 nanoseconds. Applies to: ace 2 GigE | |
Within100us | The expected accuracy of the PTP device clock is within 100 microseconds. Applies to: ace 2 GigE | |
Within10ms | The expected accuracy of the PTP device clock is within 10 milliseconds. Applies to: ace 2 GigE | |
Within10s | The expected accuracy of the PTP device clock is within 10 seconds. Applies to: ace 2 GigE | |
Within10us | The expected accuracy of the PTP device clock is within 10 microseconds. Applies to: ace 2 GigE | |
Within1ms | The expected accuracy of the PTP device clock is within 1 millisecond. Applies to: ace 2 GigE | |
Within1s | The expected accuracy of the PTP device clock is within 1 second. Applies to: ace 2 GigE | |
Within1us | The expected accuracy of the PTP device clock is within 1 microsecond. Applies to: ace 2 GigE | |
Within250ms | The expected accuracy of the PTP device clock is within 250 milliseconds. Applies to: ace 2 GigE | |
Within250ns | The expected accuracy of the PTP device clock is within 250 nanoseconds. Applies to: ace 2 GigE | |
Within250us | The expected accuracy of the PTP device clock is within 250 microseconds. Applies to: ace 2 GigE | |
Within25ms | The expected accuracy of the PTP device clock is within 25 milliseconds. Applies to: ace 2 GigE | |
Within25ns | The expected accuracy of the PTP device clock is within 25 nanoseconds. Applies to: ace 2 GigE | |
Within25us | The expected accuracy of the PTP device clock is within 25 microseconds. Applies to: ace 2 GigE | |
Within2p5ms | The expected accuracy of the PTP device clock is within 2.5 milliseconds. Applies to: ace 2 GigE | |
Within2p5us | The expected accuracy of the PTP device clock is within 2.5 microseconds. Applies to: ace 2 GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of PtpClockAccuracy (Overrides Object.ToString()()()().) |
PLCamera.PtpClockAccuracyEnum.ToString Method#
The full name of PtpClockAccuracy
Return Value#
Type: String
Returns the full name of PtpClockAccuracy
PLCamera.PtpClockAccuracyEnum Constructor#
Initializes a new instance of the PLCamera.PtpClockAccuracyEnum class
PLCamera.PtpClockAccuracyEnum.GreaterThan10s Property#
The expected accuracy of the PTP device clock is greater than 10 seconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Name Property#
The full name of PtpClockAccuracy
PLCamera.PtpClockAccuracyEnum.Unknown Property#
The expected accuracy of the PTP device clock is unknown.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within100ms Property#
The expected accuracy of the PTP device clock is within 100 milliseconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within100ns Property#
The expected accuracy of the PTP device clock is within 100 nanoseconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within100us Property#
The expected accuracy of the PTP device clock is within 100 microseconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within10ms Property#
The expected accuracy of the PTP device clock is within 10 milliseconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within10s Property#
The expected accuracy of the PTP device clock is within 10 seconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within10us Property#
The expected accuracy of the PTP device clock is within 10 microseconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within1ms Property#
The expected accuracy of the PTP device clock is within 1 millisecond.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within1s Property#
The expected accuracy of the PTP device clock is within 1 second.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within1us Property#
The expected accuracy of the PTP device clock is within 1 microsecond.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within250ms Property#
The expected accuracy of the PTP device clock is within 250 milliseconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within250ns Property#
The expected accuracy of the PTP device clock is within 250 nanoseconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within250us Property#
The expected accuracy of the PTP device clock is within 250 microseconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within25ms Property#
The expected accuracy of the PTP device clock is within 25 milliseconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within25ns Property#
The expected accuracy of the PTP device clock is within 25 nanoseconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within25us Property#
The expected accuracy of the PTP device clock is within 25 microseconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within2p5ms Property#
The expected accuracy of the PTP device clock is within 2.5 milliseconds.
Applies to: ace 2 GigE
PLCamera.PtpClockAccuracyEnum.Within2p5us Property#
The expected accuracy of the PTP device clock is within 2.5 microseconds.
Applies to: ace 2 GigE