PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum Class#
Applies to: boost_V_CoaXPress
Visibility: Expert
Selecting Parameters: BslStaticDefectPixelCorrectionXCoordinate
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum | Initializes a new instance of the PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of BslStaticDefectPixelCorrectionXSelector (Overrides ParameterListEnum.Name.) | |
X0 | Entry X0 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry. Applies to: boost_V_CoaXPress | |
X1 | Entry X1 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry. Applies to: boost_V_CoaXPress | |
X2 | Entry X2 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry. Applies to: boost_V_CoaXPress | |
X3 | Entry X3 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry. Applies to: boost_V_CoaXPress | |
X4 | Entry X4 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry. Applies to: boost_V_CoaXPress | |
X5 | Entry X5 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry. Applies to: boost_V_CoaXPress | |
X6 | Entry X6 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry. Applies to: boost_V_CoaXPress | |
X7 | Entry X7 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry. Applies to: boost_V_CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslStaticDefectPixelCorrectionXSelector (Overrides Object.ToString()()()().) |
PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.ToString Method#
The full name of BslStaticDefectPixelCorrectionXSelector
Return Value#
Type: String
Returns the full name of BslStaticDefectPixelCorrectionXSelector
PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum Constructor#
Initializes a new instance of the PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum class
PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.Name Property#
The full name of BslStaticDefectPixelCorrectionXSelector
PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X0 Property#
Entry X0 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.
Applies to: boost_V_CoaXPress
PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X1 Property#
Entry X1 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.
Applies to: boost_V_CoaXPress
PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X2 Property#
Entry X2 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.
Applies to: boost_V_CoaXPress
PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X3 Property#
Entry X3 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.
Applies to: boost_V_CoaXPress
PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X4 Property#
Entry X4 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.
Applies to: boost_V_CoaXPress
PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X5 Property#
Entry X5 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.
Applies to: boost_V_CoaXPress
PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X6 Property#
Entry X6 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.
Applies to: boost_V_CoaXPress
PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X7 Property#
Entry X7 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.
Applies to: boost_V_CoaXPress