PLCamera.ImageCompressionModeEnum Class#
Applies to: ace 2 GigE and ace 2 USB
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ImageCompressionModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.ImageCompressionModeEnum | Initializes a new instance of the PLCamera.ImageCompressionModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
BaslerCompressionBeyond | Images are compressed using the Compression Beyond feature. Applies to: ace 2 GigE and ace 2 USB | |
名前 | The full name of ImageCompressionMode (Overrides ParameterListEnum.Name.) | |
Off | Image compression is disabled. The image is transmitted uncompressed. Applies to: ace 2 GigE and ace 2 USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of ImageCompressionMode (Overrides Object.ToString()()()().) |
PLCamera.ImageCompressionModeEnum.ToString Method#
The full name of ImageCompressionMode
Return Value#
Type: String
Returns the full name of ImageCompressionMode
PLCamera.ImageCompressionModeEnum Constructor#
Initializes a new instance of the PLCamera.ImageCompressionModeEnum class
PLCamera.ImageCompressionModeEnum.BaslerCompressionBeyond Property#
Images are compressed using the Compression Beyond feature.
Applies to: ace 2 GigE and ace 2 USB
PLCamera.ImageCompressionModeEnum.Name Property#
The full name of ImageCompressionMode
PLCamera.ImageCompressionModeEnum.Off Property#
Image compression is disabled. The image is transmitted uncompressed.
Applies to: ace 2 GigE and ace 2 USB