PLCamera.DeviceTapGeometryEnum Class#
Applies to: boost CoaXPress and boost_V_CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.DeviceTapGeometryEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.DeviceTapGeometryEnum | Initializes a new instance of the PLCamera.DeviceTapGeometryEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Geometry_1X_1Y | The tap geometry is set to 1 zone in horizontal direction with one tap and 1 zone in vertical direction with 1 tap. Applies to: boost CoaXPress and boost_V_CoaXPress | |
Geometry_1X_2YE | The tap geometry is set to 1 zone in horizontal direction with one tap and 2 zones in vertical direction with 1 tap with end extraction. Applies to: boost_V_CoaXPress | |
名前 | The full name of DeviceTapGeometry (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of DeviceTapGeometry (Overrides Object.ToString()()()().) |
PLCamera.DeviceTapGeometryEnum.ToString Method#
The full name of DeviceTapGeometry
Return Value#
Type: String
Returns the full name of DeviceTapGeometry
PLCamera.DeviceTapGeometryEnum Constructor#
Initializes a new instance of the PLCamera.DeviceTapGeometryEnum class
PLCamera.DeviceTapGeometryEnum.Geometry_1X_1Y Property#
The tap geometry is set to 1 zone in horizontal direction with one tap and 1 zone in vertical direction with 1 tap.
Applies to: boost CoaXPress and boost_V_CoaXPress
PLCamera.DeviceTapGeometryEnum.Geometry_1X_2YE Property#
The tap geometry is set to 1 zone in horizontal direction with one tap and 2 zones in vertical direction with 1 tap with end extraction.
Applies to: boost_V_CoaXPress
PLCamera.DeviceTapGeometryEnum.Name Property#
The full name of DeviceTapGeometry