GenApiノードの参照クラス#
ファイル#
名前 |
---|
GenApi/Container.h Portable container classes for INode & IValue pointers. |
GenApi/NodeCallback.h Implementation helpers for CNodeCallback Defines a bunch of templates for creating callback-functors taking a INode pointer and returning void. |
クラス#
名前 | |
---|---|
class | GenApi::node_vector A vector of INode pointers. |
class | GenApi::value_vector A vector of IValue pointers. |
struct | GenApi::IFileProtocolAdapter Adapter between the std::iostreambuf and the SFNC Features representing the device filesystem. |
struct | GenApi::ISelector Interface for groups of features selected by a single one. |
class | GenApi::CNodeCallback callback body instance for INode pointers |
class | GenApi::Function_NodeCallback Container for a function pointer. |
class | GenApi::Member_NodeCallback Container for a member function pointer. |
タイプ#
名前 | |
---|---|
enum | _ESlope |
enum | _EXMLValidation { xvLoad = 0x00000001L, xvCycles = 0x00000002L, xvSFNC = 0x00000004L, xvDefault = 0x00000000L, xvAll = 0xffffffffL, _UndefinedEXMLValidation = 0x8000000L} typedef describing the different validity checks which can be performed on an XML file |
enum | _EDisplayNotation |
enum | _EInterfaceType |
enum | _ELinkType { ctParentNodes, ctReadingChildren, ctWritingChildren, ctInvalidatingChildren, ctDependingNodes, ctTerminalNodes, ctValueChangingChildren} typedef for link type |
enum | _EIncMode |
enum | _EInputDirection |
typedef CBaseRefT< IBase > | CBaseRef |
typedef CBooleanRefT< IBoolean > | CBooleanRef |
typedef CCategoryRefT< ICategory > | CCategoryRef |
typedef CCommandRefT< ICommand > | CCommandRef |
typedef CEnumEntryRefT< IEnumEntry > | CEnumEntryRef |
typedef CFloatRefT< IFloat > | CFloatRef |
typedef CIntegerRefT< IInteger > | CIntegerRef |
typedef CPortRefT< IPort > | CPortRef |
typedef CRegisterRefT< IRegister > | CRegisterRef |
typedef CSelectorRefT< ISelector > | CSelectorRef |
typedef CStringRefT< IString > | CStringRef |
typedef CValueRefT< IValue > | CValueRef |
typedef CPointer< IPortConstruct > | CPortConstructPtr SmartPointer for IPortConstruct interface pointer. |
typedef GenICam::gcstring_vector | StringList_t |
typedef enum GenApi::_ESlope | ESlope |
typedef enum GenApi::_EXMLValidation | EXMLValidation typedef describing the different validity checks which can be performed on an XML file |
typedef enum GenApi::_EDisplayNotation | EDisplayNotation |
typedef enum GenApi::_EInterfaceType | EInterfaceType |
typedef enum GenApi::_ELinkType | ELinkType typedef for link type |
typedef enum GenApi::_EIncMode | EIncMode |
typedef enum GenApi::_EInputDirection | EInputDirection |
Functions#
名前 | |
---|---|
template <class Function > CNodeCallback * | make_NodeCallback(INode * pNode, Function function, ECallbackType CallbackType) make a new callback object for C functions |
template <class Client ,class Member > CNodeCallback * | make_NodeCallback(INode * pNode, Client & client, Member member, ECallbackType CallbackType) make a new callback object for member functions |
GenICam::gcstring | GetInterfaceName(IBase * pBase) |
template <class T ,class B > bool | IsReadable(const CPointer< T, B > & ptr) Checks if a node is readable. |
template <class T ,class B > bool | IsWritable(const CPointer< T, B > & ptr) Checks if a node is Writable. |
template <class T ,class B > bool | IsImplemented(const CPointer< T, B > & ptr) Checks if a node is Implemented. |
template <class T ,class B > bool | IsAvailable(const CPointer< T, B > & ptr) Checks if a node is Available. |
Types Documentation#
enum _ESlope#
Enumerator | 値 | 説明 |
---|---|---|
Increasing | strictly monotonous increasing | |
Decreasing | strictly monotonous decreasing | |
Varying | slope changes, e.g. at run-time | |
自動 | slope is determined automatically by probing the function | |
_UndefinedESlope | Object is not yet initialized. |
typedef for formula type
enum _EXMLValidation#
Enumerator | 値 | 説明 |
---|---|---|
xvLoad | 0x00000001L | Creates a dummy node map. |
xvCycles | 0x00000002L | checks for write and dependency cycles (implies xvLoad) |
xvSFNC | 0x00000004L | checks for conformance with the standard feature naming convention (SFNC) |
xvDefault | 0x00000000L | checks performed if nothing else is said |
xvAll | 0xffffffffL | all possible checks |
_UndefinedEXMLValidation | 0x8000000L | Object is not yet initialized. |
typedef describing the different validity checks which can be performed on an XML file
The enum values for a bitfield of length uint32_t
enum _EDisplayNotation#
Enumerator | 値 | 説明 |
---|---|---|
fnAutomatic | the notation if either scientific or fixed depending on what is shorter | |
fnFixed | the notation is fixed, e.g. 123.4 | |
fnScientific | the notation is scientific, e.g. 1.234e2 | |
_UndefinedEDisplayNotation | Object is not yet initialized. |
typedef for float notation
enum _EInterfaceType#
Enumerator | 値 | 説明 |
---|---|---|
intfIValue | IValue interface. | |
intfIBase | IBase interface. | |
intfIInteger | IInteger interface. | |
intfIBoolean | IBoolean interface. | |
intfICommand | ICommand interface. | |
intfIFloat | IFloat interface. | |
intfIString | IString interface. | |
intfIRegister | IRegister interface. | |
intfICategory | ICategory interface. | |
intfIEnumeration | IEnumeration interface. | |
intfIEnumEntry | IEnumEntry interface. | |
intfIPort | IPort interface. |
typedef for interface type
enum _ELinkType#
Enumerator | 値 | 説明 |
---|---|---|
ctParentNodes | All nodes for which this node is at least an invalidating child. | |
ctReadingChildren | All nodes which can be read from. | |
ctWritingChildren | All nodes which can write a value further down the node stack. | |
ctInvalidatingChildren | All directly connected nodes which invalidate this node. | |
ctDependingNodes | All directly or indirectly connected nodes which are invalidated by this nodes (i.e. which are dependent on this node) | |
ctTerminalNodes | All indirectly connected terminal nodes. | |
ctValueChangingChildren | All child node used to compute the value. |
typedef for link type
For details see GenICam Wiki : GenApi/SoftwareArchitecture/NodeDependencies
enum _EIncMode#
Enumerator | 値 | 説明 |
---|---|---|
noIncrement | ||
fixedIncrement | ||
listIncrement |
typedef for increment mode
enum _EInputDirection#
Enumerator | 値 | 説明 |
---|---|---|
idFrom | Indicates a swiss knife that it is used as worker for a converter computing FROM. | |
idTo | Indicates a swiss knife that it is used as worker for a converter computing TO. | |
idNone | SwissKnife is not used within a converter. |
typedef for link type
typedef CBaseRef#
Reference to an IBase pointer
typedef CBooleanRef#
Reference to an IBoolean pointer
typedef CCategoryRef#
Reference to an ICategory pointer
typedef CCommandRef#
Reference to an ICommand pointer
typedef CEnumEntryRef#
Reference to an IEnumEntry pointer
typedef CFloatRef#
Reference to an IFloat pointer
typedef CIntegerRef#
Reference to an IInteger pointer
typedef CPortRef#
Reference to an IEnumEntry pointer
typedef CRegisterRef#
Reference to an IRegister pointer
typedef CSelectorRef#
Reference to an ISelector pointer
typedef CStringRef#
Reference to an IString pointer
typedef CValueRef#
Reference to an IValue pointer
typedef CPortConstructPtr#
SmartPointer for IPortConstruct interface pointer.
typedef StringList_t#
A list of strings
typedef ESlope#
typedef for formula type
typedef EXMLValidation#
typedef describing the different validity checks which can be performed on an XML file
The enum values for a bitfield of length uint32_t
typedef EDisplayNotation#
typedef for float notation
typedef EInterfaceType#
typedef for interface type
typedef ELinkType#
typedef for link type
For details see GenICam Wiki : GenApi/SoftwareArchitecture/NodeDependencies
typedef EIncMode#
typedef for increment mode
typedef EInputDirection#
typedef for link type
Functions Documentation#
function make_NodeCallback#
template <class Function >
CNodeCallback * make_NodeCallback(
INode * pNode,
Function function,
ECallbackType CallbackType
)
make a new callback object for C functions
function make_NodeCallback#
template <class Client ,
class Member >
CNodeCallback * make_NodeCallback(
INode * pNode,
Client & client,
Member member,
ECallbackType CallbackType
)
make a new callback object for member functions
function GetInterfaceName#
Returns the name of the main interface as string DEPRECATED, use IBase::GetPrincipalInterfaceType() instead
function IsReadable#
Checks if a node is readable.
function IsWritable#
Checks if a node is Writable.
function IsImplemented#
Checks if a node is Implemented.
function IsAvailable#
Checks if a node is Available.