PLCamera.ParameterSelectorEnum Class#
Applies to: CameraLink and GigE
Visibility: Guru
Selecting Parameters: RemoveLimits
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ParameterSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.ParameterSelectorEnum | Initializes a new instance of the PLCamera.ParameterSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
AutoTargetValue | The factory limits of the Auto Target Value parameter can be removed. Applies to: CameraLink and GigE | |
BlackLevel | The factory limits of the Black Level parameter can be removed. Applies to: CameraLink and GigE | |
明るさ | The factory limits of the Brightness parameter can be removed. Applies to: CameraLink and GigE | |
ExposureOverhead | The factory limits of the Exposure Overhead parameter can be removed. Applies to: CameraLink and GigE | |
ExposureOverlapMax | The factory limits of the Exposure Overlap Time Max parameter can be removed. Applies to: GigE | |
ExposureTime | The factory limits of the Exposure Time parameter can be removed. Applies to: CameraLink and GigE | |
Framerate | The factory limits of the Framerate parameter can be removed. Applies to: CameraLink and GigE | |
Gain | The factory limits of the Gain parameter can be removed. Applies to: CameraLink and GigE | |
名前 | The full name of ParameterSelector (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of ParameterSelector (Overrides Object.ToString()()()().) |
PLCamera.ParameterSelectorEnum.ToString Method#
The full name of ParameterSelector
Return Value#
Type: String
Returns the full name of ParameterSelector
PLCamera.ParameterSelectorEnum Constructor#
Initializes a new instance of the PLCamera.ParameterSelectorEnum class
PLCamera.ParameterSelectorEnum.AutoTargetValue Property#
The factory limits of the Auto Target Value parameter can be removed.
Applies to: CameraLink and GigE
PLCamera.ParameterSelectorEnum.BlackLevel Property#
The factory limits of the Black Level parameter can be removed.
Applies to: CameraLink and GigE
PLCamera.ParameterSelectorEnum.Brightness Property#
The factory limits of the Brightness parameter can be removed.
Applies to: CameraLink and GigE
PLCamera.ParameterSelectorEnum.ExposureOverhead Property#
The factory limits of the Exposure Overhead parameter can be removed.
Applies to: CameraLink and GigE
PLCamera.ParameterSelectorEnum.ExposureOverlapMax Property#
The factory limits of the Exposure Overlap Time Max parameter can be removed.
Applies to: GigE
PLCamera.ParameterSelectorEnum.ExposureTime Property#
The factory limits of the Exposure Time parameter can be removed.
Applies to: CameraLink and GigE
PLCamera.ParameterSelectorEnum.Framerate Property#
The factory limits of the Framerate parameter can be removed.
Applies to: CameraLink and GigE
PLCamera.ParameterSelectorEnum.Gain Property#
The factory limits of the Gain parameter can be removed.
Applies to: CameraLink and GigE
PLCamera.ParameterSelectorEnum.Name Property#
The full name of ParameterSelector