PLEventGrabber.StatusEnum Class#
Applies to: GigE
Visibility: Guru
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLEventGrabber.StatusEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLEventGrabber.StatusEnum | Initializes a new instance of the PLEventGrabber.StatusEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Closed | The low level event grabber is closed. Applies to: GigE | |
名前 | The full name of Status (Overrides ParameterListEnum.Name.) | |
Open | The low level event grabber is open. Applies to: GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of Status (Overrides Object.ToString()()()().) |
PLEventGrabber.StatusEnum.ToString Method#
The full name of Status
Return Value#
Type: String
Returns the full name of Status
PLEventGrabber.StatusEnum Constructor#
Initializes a new instance of the PLEventGrabber.StatusEnum class
PLEventGrabber.StatusEnum.Closed Property#
The low level event grabber is closed.
Applies to: GigE
PLEventGrabber.StatusEnum.Name Property#
The full name of Status
PLEventGrabber.StatusEnum.Open Property#
The low level event grabber is open.
Applies to: GigE