PLCamera.FileOperationSelectorEnum Class#
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
Visibility: Guru
Selected by: FileSelector
Selecting Parameters: FileAccessLength, FileAccessOffset, FileOperationExecute, FileOperationResult, FileOperationStatus
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.FileOperationSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.FileOperationSelectorEnum | Initializes a new instance of the PLCamera.FileOperationSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Close | Basler advises against using this parameter. Use the appropriate feature for file access operations instead. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
名前 | The full name of FileOperationSelector (Overrides ParameterListEnum.Name.) | |
Open | Basler advises against using this parameter. Use the appropriate feature for file access operations instead. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
読み取り | Basler advises against using this parameter. Use the appropriate feature for file access operations instead. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
Write | Basler advises against using this parameter. Use the appropriate feature for file access operations instead. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of FileOperationSelector (Overrides Object.ToString()()()().) |
PLCamera.FileOperationSelectorEnum.ToString Method#
The full name of FileOperationSelector
Return Value#
Type: String
Returns the full name of FileOperationSelector
PLCamera.FileOperationSelectorEnum Constructor#
Initializes a new instance of the PLCamera.FileOperationSelectorEnum class
PLCamera.FileOperationSelectorEnum.Close Property#
Basler advises against using this parameter. Use the appropriate feature for file access operations instead.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.FileOperationSelectorEnum.Name Property#
The full name of FileOperationSelector
PLCamera.FileOperationSelectorEnum.Open Property#
Basler advises against using this parameter. Use the appropriate feature for file access operations instead.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.FileOperationSelectorEnum.Read Property#
Basler advises against using this parameter. Use the appropriate feature for file access operations instead.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.FileOperationSelectorEnum.Write Property#
Basler advises against using this parameter. Use the appropriate feature for file access operations instead.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB