PLCamera.CxpErrorCounterSelectorEnum Class#
Applies to: boost CoaXPress
Visibility: Expert
Selected by: CxpConnectionSelector
Selecting Parameters: CxpErrorCounterReset, CxpErrorCounterStatus, CxpErrorCounterValue
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.CxpErrorCounterSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.CxpErrorCounterSelectorEnum | Initializes a new instance of the PLCamera.CxpErrorCounterSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
ConnectionLockLoss | The Connection Lock Loss error counter can be read or reset. Applies to: boost CoaXPress | |
ControlPacketCrc | The Control Packet CRC error counter can be read or reset. Applies to: boost CoaXPress | |
DuplicatedCharactersUncorrected | The Duplicated Characters Uncorrected error counter can be read or reset. Applies to: boost CoaXPress | |
名前 | The full name of CxpErrorCounterSelector (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of CxpErrorCounterSelector (Overrides Object.ToString()()()().) |
PLCamera.CxpErrorCounterSelectorEnum.ToString Method#
The full name of CxpErrorCounterSelector
Return Value#
Type: String
Returns the full name of CxpErrorCounterSelector
PLCamera.CxpErrorCounterSelectorEnum Constructor#
Initializes a new instance of the PLCamera.CxpErrorCounterSelectorEnum class
PLCamera.CxpErrorCounterSelectorEnum.ConnectionLockLoss Property#
The Connection Lock Loss error counter can be read or reset.
Applies to: boost CoaXPress
PLCamera.CxpErrorCounterSelectorEnum.ControlPacketCrc Property#
The Control Packet CRC error counter can be read or reset.
Applies to: boost CoaXPress
PLCamera.CxpErrorCounterSelectorEnum.DuplicatedCharactersUncorrected Property#
The Duplicated Characters Uncorrected error counter can be read or reset.
Applies to: boost CoaXPress
PLCamera.CxpErrorCounterSelectorEnum.Name Property#
The full name of CxpErrorCounterSelector