PLCamera.TimerSelectorEnum Class#
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
Visibility: Beginner
Selecting Parameters: TimerDelay, TimerDelayAbs, TimerDelayRaw, TimerDuration, TimerDurationAbs, TimerDurationRaw, TimerReset, TimerStatus, TimerTriggerActivation, TimerTriggerArmDelay, TimerTriggerSource
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.TimerSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.TimerSelectorEnum | Initializes a new instance of the PLCamera.TimerSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of TimerSelector (Overrides ParameterListEnum.Name.) | |
Timer1 | Timer 1 can be configured. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
Timer2 | Timer 2 can be configured. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Timer3 | Timer 3 can be configured. Applies to: CameraLink and GigE | |
Timer4 | Timer 4 can be configured. Applies to: CameraLink and GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of TimerSelector (Overrides Object.ToString()()()().) |
PLCamera.TimerSelectorEnum.ToString Method#
The full name of TimerSelector
Return Value#
Type: String
Returns the full name of TimerSelector
PLCamera.TimerSelectorEnum Constructor#
Initializes a new instance of the PLCamera.TimerSelectorEnum class
PLCamera.TimerSelectorEnum.Name Property#
The full name of TimerSelector
PLCamera.TimerSelectorEnum.Timer1 Property#
Timer 1 can be configured.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.TimerSelectorEnum.Timer2 Property#
Timer 2 can be configured.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.TimerSelectorEnum.Timer3 Property#
Timer 3 can be configured.
Applies to: CameraLink and GigE
PLCamera.TimerSelectorEnum.Timer4 Property#
Timer 4 can be configured.
Applies to: CameraLink and GigE