PLCamera.LineSourceEnum Class#
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB and dart USB
Visibility: Beginner
Selected by: LineSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.LineSourceEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.LineSourceEnum | Initializes a new instance of the PLCamera.LineSourceEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
AcquisitionActive | The source signal for the currently selected line is set to Acquisition Active. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
AcquisitionTriggerReady | The source signal for the currently selected line is set to Acquisition Trigger Ready. Applies to: CameraLink and GigE | |
AcquisitionTriggerWait | The source signal for the currently selected line is set to Acquisition Trigger Wait. Applies to: CameraLink and GigE | |
BslLightControl | The source signal for the currently selected line is set to Light Control. If you change this setting, your light will stop working. Applies to: GigE and ace USB | |
Counter1Active | The source signal for the currently selected line is set to Counter 1 Active. The signal goes high when the counter is started. The signal goes low when the counter is stopped, reset, or when it has reached its maximum value. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Counter2Active | The source signal for the currently selected line is set to Counter 2 Active. The signal goes high when the counter is started. The signal goes low when the counter is stopped, reset, or when it has reached its maximum value. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
ExposureActive | The source signal for the currently selected line is set to Exposure Active. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB and dart USB | |
ExposureTriggerWait | The source signal for the currently selected line is set to Exposure Trigger Wait. The signal goes high when the camera is ready to receive exposure trigger signals. When you apply an exposure trigger signal, the signal goes low. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
FlashWindow | The source signal for the currently selected line is set to Flash Window. Applies to: CameraLink, GigE, ace USB and dart USB | |
FrameBurstActive | The source signal for the currently selected line is set to Frame Burst Active. You can use this signal to monitor if the camera is currently acquiring a series of images (a "burst" of images). The signal goes high when the acquisition of a series of images has started. The signal goes low when the acquisition of a series of images has finished. Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
FrameBurstTriggerWait | The source signal for the currently selected line is set to Frame Burst Trigger Wait. Applies to: CamEmu, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
FrameCycle | The signal for the currently selected line is rising with Frame Trigger Wait and falling with Exposure Active. Applies to: CameraLink and GigE | |
FrameTriggerWait | The source signal for the currently selected line is set to Frame Trigger Wait. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
FrequencyConverter | The signal for the currently selected line is associated with the output of the frequency converter module. Applies to: CameraLink and GigE | |
LineTriggerWait | The source signal for the currently selected line is set to Line Trigger Wait. Applies to: CameraLink and GigE | |
名前 | The full name of LineSource (Overrides ParameterListEnum.Name.) | |
Off | No source signal is set for the currently selected line. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB | |
PatternGenerator1 | Applies to: CameraLink and GigE | |
PatternGenerator2 | Applies to: CameraLink and GigE | |
PatternGenerator3 | Applies to: CameraLink and GigE | |
PatternGenerator4 | Applies to: CameraLink and GigE | |
SerialTx | The source signal for the currently selected line is set to Serial Tx. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB and boost CoaXPress | |
ShaftEncoderModuleOut | The signal for the currently selected line is associated with the output of the shaft encoder module. Applies to: CameraLink and GigE | |
SyncUserOutput | The source signal for the currently selected line is set to Sync User Output. Applies to: CameraLink and GigE | |
SyncUserOutput0 | The source signal for the currently selected line is set to Sync User Output 0. Applies to: GigE | |
SyncUserOutput1 | The source signal for the currently selected line is set to Sync User Output 1. Applies to: GigE | |
SyncUserOutput2 | The source signal for the currently selected line is set to Sync User Output 2. Applies to: GigE | |
SyncUserOutput3 | The source signal for the currently selected line is set to Sync User Output 3. Applies to: GigE | |
Timer1Active | The source signal for the currently selected line is set to Timer 1 Active. You can use this signal to monitor the camera's Timer feature. The signal goes high after the delay specified. The signal goes low after the duration specified. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
Timer2Active | The source signal for the currently selected line is set to Timer 2 Active. You can use this signal to monitor the camera's Timer feature. The signal goes high after the delay specified. The signal goes low after the duration specified. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Timer3Active | This enumeration value sets the source signal for the selected output line to timer 3 active. Applies to: CameraLink and GigE | |
Timer4Active | This enumeration value sets the source signal for the selected output line to timer 4 active. Applies to: CameraLink and GigE | |
TimerActive | The source signal for the currently selected line is set to Timer Active. Applies to: CameraLink and GigE | |
TriggerReady | The source signal for the currently selected line is set to Trigger Ready. Applies to: CameraLink and GigE | |
UserOutput | The source signal for the currently selected line is set to User Output. Applies to: CameraLink and GigE | |
UserOutput0 | The source signal for the currently selected line is set to User Output 0. Applies to: GigE and ace USB | |
UserOutput1 | The source signal for the currently selected line is set to User Output 1. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB | |
UserOutput2 | The source signal for the currently selected line is set to User Output 2. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB | |
UserOutput3 | The source signal for the currently selected line is set to User Output 3. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB | |
UserOutput4 | The source signal for the currently selected line is set to User Output 4. Applies to: CameraLink, GigE, dart 2 USB and dart USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of LineSource (Overrides Object.ToString()()()().) |
PLCamera.LineSourceEnum.ToString Method#
The full name of LineSource
Return Value#
Type: String
Returns the full name of LineSource
PLCamera.LineSourceEnum Constructor#
Initializes a new instance of the PLCamera.LineSourceEnum class
PLCamera.LineSourceEnum.AcquisitionActive Property#
The source signal for the currently selected line is set to Acquisition Active.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.LineSourceEnum.AcquisitionTriggerReady Property#
The source signal for the currently selected line is set to Acquisition Trigger Ready.
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.AcquisitionTriggerWait Property#
The source signal for the currently selected line is set to Acquisition Trigger Wait.
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.BslLightControl Property#
The source signal for the currently selected line is set to Light Control. If you change this setting, your light will stop working.
Applies to: GigE and ace USB
PLCamera.LineSourceEnum.Counter1Active Property#
The source signal for the currently selected line is set to Counter 1 Active. The signal goes high when the counter is started. The signal goes low when the counter is stopped, reset, or when it has reached its maximum value.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.LineSourceEnum.Counter2Active Property#
The source signal for the currently selected line is set to Counter 2 Active. The signal goes high when the counter is started. The signal goes low when the counter is stopped, reset, or when it has reached its maximum value.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.LineSourceEnum.ExposureActive Property#
The source signal for the currently selected line is set to Exposure Active.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress, dart 2 USB and dart USB
PLCamera.LineSourceEnum.ExposureTriggerWait Property#
The source signal for the currently selected line is set to Exposure Trigger Wait. The signal goes high when the camera is ready to receive exposure trigger signals. When you apply an exposure trigger signal, the signal goes low.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.LineSourceEnum.FlashWindow Property#
The source signal for the currently selected line is set to Flash Window.
Applies to: CameraLink, GigE, ace USB and dart USB
PLCamera.LineSourceEnum.FrameBurstActive Property#
The source signal for the currently selected line is set to Frame Burst Active. You can use this signal to monitor if the camera is currently acquiring a series of images (a "burst" of images). The signal goes high when the acquisition of a series of images has started. The signal goes low when the acquisition of a series of images has finished.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.LineSourceEnum.FrameBurstTriggerWait Property#
The source signal for the currently selected line is set to Frame Burst Trigger Wait.
Applies to: CamEmu, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.LineSourceEnum.FrameCycle Property#
The signal for the currently selected line is rising with Frame Trigger Wait and falling with Exposure Active.
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.FrameTriggerWait Property#
The source signal for the currently selected line is set to Frame Trigger Wait.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.LineSourceEnum.FrequencyConverter Property#
The signal for the currently selected line is associated with the output of the frequency converter module.
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.LineTriggerWait Property#
The source signal for the currently selected line is set to Line Trigger Wait.
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.Name Property#
The full name of LineSource
PLCamera.LineSourceEnum.Off Property#
No source signal is set for the currently selected line.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB
PLCamera.LineSourceEnum.PatternGenerator1 Property#
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.PatternGenerator2 Property#
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.PatternGenerator3 Property#
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.PatternGenerator4 Property#
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.SerialTx Property#
The source signal for the currently selected line is set to Serial Tx.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.LineSourceEnum.ShaftEncoderModuleOut Property#
The signal for the currently selected line is associated with the output of the shaft encoder module.
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.SyncUserOutput Property#
The source signal for the currently selected line is set to Sync User Output.
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.SyncUserOutput0 Property#
The source signal for the currently selected line is set to Sync User Output 0.
Applies to: GigE
PLCamera.LineSourceEnum.SyncUserOutput1 Property#
The source signal for the currently selected line is set to Sync User Output 1.
Applies to: GigE
PLCamera.LineSourceEnum.SyncUserOutput2 Property#
The source signal for the currently selected line is set to Sync User Output 2.
Applies to: GigE
PLCamera.LineSourceEnum.SyncUserOutput3 Property#
The source signal for the currently selected line is set to Sync User Output 3.
Applies to: GigE
PLCamera.LineSourceEnum.Timer1Active Property#
The source signal for the currently selected line is set to Timer 1 Active. You can use this signal to monitor the camera's Timer feature. The signal goes high after the delay specified. The signal goes low after the duration specified.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.LineSourceEnum.Timer2Active Property#
The source signal for the currently selected line is set to Timer 2 Active. You can use this signal to monitor the camera's Timer feature. The signal goes high after the delay specified. The signal goes low after the duration specified.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.LineSourceEnum.Timer3Active Property#
This enumeration value sets the source signal for the selected output line to timer 3 active.
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.Timer4Active Property#
This enumeration value sets the source signal for the selected output line to timer 4 active.
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.TimerActive Property#
The source signal for the currently selected line is set to Timer Active.
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.TriggerReady Property#
The source signal for the currently selected line is set to Trigger Ready.
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.UserOutput Property#
The source signal for the currently selected line is set to User Output.
Applies to: CameraLink and GigE
PLCamera.LineSourceEnum.UserOutput0 Property#
The source signal for the currently selected line is set to User Output 0.
Applies to: GigE and ace USB
PLCamera.LineSourceEnum.UserOutput1 Property#
The source signal for the currently selected line is set to User Output 1.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB
PLCamera.LineSourceEnum.UserOutput2 Property#
The source signal for the currently selected line is set to User Output 2.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB
PLCamera.LineSourceEnum.UserOutput3 Property#
The source signal for the currently selected line is set to User Output 3.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB and dart USB
PLCamera.LineSourceEnum.UserOutput4 Property#
The source signal for the currently selected line is set to User Output 4.
Applies to: CameraLink, GigE, dart 2 USB and dart USB