PLCamera.ClTimeSlotsEnum Class#
Applies to: CameraLink
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ClTimeSlotsEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.ClTimeSlotsEnum | Initializes a new instance of the PLCamera.ClTimeSlotsEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of ClTimeSlots (Overrides ParameterListEnum.Name.) | |
TimeSlots1 | The time slot is set to one time slot. Applies to: CameraLink |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of ClTimeSlots (Overrides Object.ToString()()()().) |
PLCamera.ClTimeSlotsEnum.ToString Method#
The full name of ClTimeSlots
Return Value#
Type: String
Returns the full name of ClTimeSlots
PLCamera.ClTimeSlotsEnum Constructor#
Initializes a new instance of the PLCamera.ClTimeSlotsEnum class
PLCamera.ClTimeSlotsEnum.Name Property#
The full name of ClTimeSlots
PLCamera.ClTimeSlotsEnum.TimeSlots1 Property#
The time slot is set to one time slot.
Applies to: CameraLink