PLCamera.BslUSBPowerSourceEnum Class#
Applies to: ace 2 USB
Visibility: Guru
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslUSBPowerSourceEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslUSBPowerSourceEnum | Initializes a new instance of the PLCamera.BslUSBPowerSourceEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Aux | Power is supplied via the I/O connector. Applies to: ace 2 USB | |
Bus | Power is supplied via the bus. Applies to: ace 2 USB | |
名前 | The full name of BslUSBPowerSource (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslUSBPowerSource (Overrides Object.ToString()()()().) |
PLCamera.BslUSBPowerSourceEnum.ToString Method#
The full name of BslUSBPowerSource
Return Value#
Type: String
Returns the full name of BslUSBPowerSource
PLCamera.BslUSBPowerSourceEnum Constructor#
Initializes a new instance of the PLCamera.BslUSBPowerSourceEnum class
PLCamera.BslUSBPowerSourceEnum.Aux Property#
Power is supplied via the I/O connector.
Applies to: ace 2 USB
PLCamera.BslUSBPowerSourceEnum.Bus Property#
Power is supplied via the bus.
Applies to: ace 2 USB
PLCamera.BslUSBPowerSourceEnum.Name Property#
The full name of BslUSBPowerSource