PLTransportLayer.TriggerOutputEventSelectEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.TriggerOutputEventSelectEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLTransportLayer.TriggerOutputEventSelectEnum | Initializes a new instance of the PLTransportLayer.TriggerOutputEventSelectEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of TriggerOutputEventSelect (Overrides ParameterListEnum.Name.) | |
PulseGenerator0 | The source for the output statistics is set to Pulse Generator 0. Applies to: CoaXPress | |
PulseGenerator1 | The source for the output statistics is set to Pulse Generator 1. Applies to: CoaXPress | |
PulseGenerator2 | The source for the output statistics is set to Pulse Generator 2. Applies to: CoaXPress | |
PulseGenerator3 | The source for the output statistics is set to Pulse Generator 3. Applies to: CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of TriggerOutputEventSelect (Overrides Object.ToString()()()().) |
PLTransportLayer.TriggerOutputEventSelectEnum.ToString Method#
The full name of TriggerOutputEventSelect
Return Value#
Type: String
Returns the full name of TriggerOutputEventSelect
PLTransportLayer.TriggerOutputEventSelectEnum Constructor#
Initializes a new instance of the PLTransportLayer.TriggerOutputEventSelectEnum class
PLTransportLayer.TriggerOutputEventSelectEnum.Name Property#
The full name of TriggerOutputEventSelect
PLTransportLayer.TriggerOutputEventSelectEnum.PulseGenerator0 Property#
The source for the output statistics is set to Pulse Generator 0.
Applies to: CoaXPress
PLTransportLayer.TriggerOutputEventSelectEnum.PulseGenerator1 Property#
The source for the output statistics is set to Pulse Generator 1.
Applies to: CoaXPress
PLTransportLayer.TriggerOutputEventSelectEnum.PulseGenerator2 Property#
The source for the output statistics is set to Pulse Generator 2.
Applies to: CoaXPress
PLTransportLayer.TriggerOutputEventSelectEnum.PulseGenerator3 Property#
The source for the output statistics is set to Pulse Generator 3.
Applies to: CoaXPress