PLTransportLayer.TriggerExceededPeriodLimitsEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.TriggerExceededPeriodLimitsEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLTransportLayer.TriggerExceededPeriodLimitsEnum | Initializes a new instance of the PLTransportLayer.TriggerExceededPeriodLimitsEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of TriggerExceededPeriodLimits (Overrides ParameterListEnum.Name.) | |
いいえ | The input signal frequency hasn't exceeded the maximum frequency defined by the Trigger Output Frequency parameter. Applies to: CoaXPress | |
はい | The input signal frequency has exceeded the maximum frequency defined by the Trigger Output Frequency parameter. Applies to: CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of TriggerExceededPeriodLimits (Overrides Object.ToString()()()().) |
PLTransportLayer.TriggerExceededPeriodLimitsEnum.ToString Method#
The full name of TriggerExceededPeriodLimits
Return Value#
Type: String
Returns the full name of TriggerExceededPeriodLimits
PLTransportLayer.TriggerExceededPeriodLimitsEnum Constructor#
Initializes a new instance of the PLTransportLayer.TriggerExceededPeriodLimitsEnum class
PLTransportLayer.TriggerExceededPeriodLimitsEnum.Name Property#
The full name of TriggerExceededPeriodLimits
PLTransportLayer.TriggerExceededPeriodLimitsEnum.No Property#
The input signal frequency hasn't exceeded the maximum frequency defined by the Trigger Output Frequency parameter.
Applies to: CoaXPress
PLTransportLayer.TriggerExceededPeriodLimitsEnum.Yes Property#
The input signal frequency has exceeded the maximum frequency defined by the Trigger Output Frequency parameter.
Applies to: CoaXPress