PLCamera.BslLightDeviceChangeIDEnum Class#
Applies to: GigE and ace USB
Visibility: Expert
Selected by: BslLightDeviceSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslLightDeviceChangeIDEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslLightDeviceChangeIDEnum | Initializes a new instance of the PLCamera.BslLightDeviceChangeIDEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Device1 | The ID of the currently selected light device is changed to Device 1. Applies to: GigE and ace USB | |
Device2 | The ID of the currently selected light device is changed to Device 2. Applies to: GigE and ace USB | |
Device3 | The ID of the currently selected light device is changed to Device 3. Applies to: GigE and ace USB | |
Device4 | The ID of the currently selected light device is changed to Device 4. Applies to: GigE and ace USB | |
名前 | The full name of BslLightDeviceChangeID (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslLightDeviceChangeID (Overrides Object.ToString()()()().) |
PLCamera.BslLightDeviceChangeIDEnum.ToString Method#
The full name of BslLightDeviceChangeID
Return Value#
Type: String
Returns the full name of BslLightDeviceChangeID
PLCamera.BslLightDeviceChangeIDEnum Constructor#
Initializes a new instance of the PLCamera.BslLightDeviceChangeIDEnum class
PLCamera.BslLightDeviceChangeIDEnum.Device1 Property#
The ID of the currently selected light device is changed to Device 1.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceChangeIDEnum.Device2 Property#
The ID of the currently selected light device is changed to Device 2.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceChangeIDEnum.Device3 Property#
The ID of the currently selected light device is changed to Device 3.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceChangeIDEnum.Device4 Property#
The ID of the currently selected light device is changed to Device 4.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceChangeIDEnum.Name Property#
The full name of BslLightDeviceChangeID