PLPixelDataConverter.MonoConversionMethodEnum Class#
Visibility: Beginner
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLPixelDataConverter.MonoConversionMethodEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLPixelDataConverter.MonoConversionMethodEnum | Initializes a new instance of the PLPixelDataConverter.MonoConversionMethodEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Gamma | When converting images, Gamma conversion is used. | |
名前 | The full name of MonoConversionMethod (Overrides ParameterListEnum.Name.) | |
Truncate | When converting images, image data is shifted. If the target bit depth is lower than the source bit depth, the least significant bits of the input pixel values are truncated. If the target bit depth is greater than the source bit depth, you can control the data alignment with the Output Bit Alignment parameter. You can use the Additional Left Shift parameter to additionally shift the input value further to the left or to the right. |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of MonoConversionMethod (Overrides Object.ToString()()()().) |
PLPixelDataConverter.MonoConversionMethodEnum.ToString Method#
The full name of MonoConversionMethod
Return Value#
Type: String
Returns the full name of MonoConversionMethod
PLPixelDataConverter.MonoConversionMethodEnum Constructor#
Initializes a new instance of the PLPixelDataConverter.MonoConversionMethodEnum class
PLPixelDataConverter.MonoConversionMethodEnum.Gamma Property#
When converting images, Gamma conversion is used.
PLPixelDataConverter.MonoConversionMethodEnum.Name Property#
The full name of MonoConversionMethod
PLPixelDataConverter.MonoConversionMethodEnum.Truncate Property#
When converting images, image data is shifted. If the target bit depth is lower than the source bit depth, the least significant bits of the input pixel values are truncated. If the target bit depth is greater than the source bit depth, you can control the data alignment with the Output Bit Alignment parameter. You can use the Additional Left Shift parameter to additionally shift the input value further to the left or to the right.