PLCamera.BslStaticDefectPixelCorrectionTestModeEnum Class#
Applies to: boost_V_CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslStaticDefectPixelCorrectionTestModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslStaticDefectPixelCorrectionTestModeEnum | Initializes a new instance of the PLCamera.BslStaticDefectPixelCorrectionTestModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of BslStaticDefectPixelCorrectionTestMode (Overrides ParameterListEnum.Name.) | |
Off | Static defect pixel correction test mode is disabled. Applies to: boost_V_CoaXPress | |
その | Static defect pixel correction test mode is enabled. All corrected pixels are set to completely white. Applies to: boost_V_CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslStaticDefectPixelCorrectionTestMode (Overrides Object.ToString()()()().) |
PLCamera.BslStaticDefectPixelCorrectionTestModeEnum.ToString Method#
The full name of BslStaticDefectPixelCorrectionTestMode
Return Value#
Type: String
Returns the full name of BslStaticDefectPixelCorrectionTestMode
PLCamera.BslStaticDefectPixelCorrectionTestModeEnum Constructor#
Initializes a new instance of the PLCamera.BslStaticDefectPixelCorrectionTestModeEnum class
PLCamera.BslStaticDefectPixelCorrectionTestModeEnum.Name Property#
The full name of BslStaticDefectPixelCorrectionTestMode
PLCamera.BslStaticDefectPixelCorrectionTestModeEnum.Off Property#
Static defect pixel correction test mode is disabled.
Applies to: boost_V_CoaXPress
PLCamera.BslStaticDefectPixelCorrectionTestModeEnum.On Property#
Static defect pixel correction test mode is enabled. All corrected pixels are set to completely white.
Applies to: boost_V_CoaXPress