PLCamera.BslLightDeviceSelectorEnum Class#
Applies to: GigE and ace USB
Visibility: Expert
Selecting Parameters: BslLightDeviceBrightness, BslLightDeviceBrightnessRaw, BslLightDeviceChangeID, BslLightDeviceClearLastError, BslLightDeviceFirmwareVersion, BslLightDeviceLastError, BslLightDeviceMaxCurrent, BslLightDeviceMaxCurrentRaw, BslLightDeviceOperationMode, BslLightDeviceStrobeDuration, BslLightDeviceStrobeDurationRaw, BslLightDeviceStrobeMode
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslLightDeviceSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslLightDeviceSelectorEnum | Initializes a new instance of the PLCamera.BslLightDeviceSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Device1 | Light device 1 can be configured. Applies to: GigE and ace USB | |
Device2 | Light device 2 can be configured. Applies to: GigE and ace USB | |
Device3 | Light device 3 can be configured. Applies to: GigE and ace USB | |
Device4 | Light device 4 can be configured. Applies to: GigE and ace USB | |
名前 | The full name of BslLightDeviceSelector (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslLightDeviceSelector (Overrides Object.ToString()()()().) |
PLCamera.BslLightDeviceSelectorEnum.ToString Method#
The full name of BslLightDeviceSelector
Return Value#
Type: String
Returns the full name of BslLightDeviceSelector
PLCamera.BslLightDeviceSelectorEnum Constructor#
Initializes a new instance of the PLCamera.BslLightDeviceSelectorEnum class
PLCamera.BslLightDeviceSelectorEnum.Device1 Property#
Light device 1 can be configured.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceSelectorEnum.Device2 Property#
Light device 2 can be configured.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceSelectorEnum.Device3 Property#
Light device 3 can be configured.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceSelectorEnum.Device4 Property#
Light device 4 can be configured.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceSelectorEnum.Name Property#
The full name of BslLightDeviceSelector