PLCamera.ComponentSelectorEnum Class#
Applies to: blaze
Visibility: Beginner
Selecting Parameters: ComponentEnable, PixelFormat
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ComponentSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.ComponentSelectorEnum | Initializes a new instance of the PLCamera.ComponentSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
信頼性 | The acquisition of confidence map of the acquired image is controlled. Confidence data may be binary (0 - invalid) or an integer where 0 is invalid and increasing value is increased confidence in the data in the corresponding pixel. If floating point representation is used the confidence image is normalized to the range [0,1], for integer representation the maximum possible integer represents maximum confidence. Applies to: blaze | |
輝度 | The acquisition of intensity (monochrome or color) of the visible reflected light is controlled. Applies to: blaze | |
名前 | The full name of ComponentSelector (Overrides ParameterListEnum.Name.) | |
範囲 | The acquisition of range (distance) data is controlled. The data produced may be only range (2.5D) or a point cloud giving the 3D coordinates depending on the Scan3dControl. Applies to: blaze |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of ComponentSelector (Overrides Object.ToString()()()().) |
PLCamera.ComponentSelectorEnum.ToString Method#
The full name of ComponentSelector
Return Value#
Type: String
Returns the full name of ComponentSelector
PLCamera.ComponentSelectorEnum Constructor#
Initializes a new instance of the PLCamera.ComponentSelectorEnum class
PLCamera.ComponentSelectorEnum.Confidence Property#
The acquisition of confidence map of the acquired image is controlled. Confidence data may be binary (0 - invalid) or an integer where 0 is invalid and increasing value is increased confidence in the data in the corresponding pixel. If floating point representation is used the confidence image is normalized to the range [0,1], for integer representation the maximum possible integer represents maximum confidence.
Applies to: blaze
PLCamera.ComponentSelectorEnum.Intensity Property#
The acquisition of intensity (monochrome or color) of the visible reflected light is controlled.
Applies to: blaze
PLCamera.ComponentSelectorEnum.Name Property#
The full name of ComponentSelector
PLCamera.ComponentSelectorEnum.Range Property#
The acquisition of range (distance) data is controlled. The data produced may be only range (2.5D) or a point cloud giving the 3D coordinates depending on the Scan3dControl.
Applies to: blaze