PLCamera.BslTemperatureStatusEnum Class#
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslTemperatureStatusEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslTemperatureStatusEnum | Initializes a new instance of the PLCamera.BslTemperatureStatusEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
重大 | The temperature is close to or at the allowed maximum. Provide cooling. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB | |
エラー | The temperature is above the allowed maximum. Provide cooling immediately. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB | |
名前 | The full name of BslTemperatureStatus (Overrides ParameterListEnum.Name.) | |
OK | The temperature is within the normal operating temperature range. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslTemperatureStatus (Overrides Object.ToString()()()().) |
PLCamera.BslTemperatureStatusEnum.ToString Method#
The full name of BslTemperatureStatus
Return Value#
Type: String
Returns the full name of BslTemperatureStatus
PLCamera.BslTemperatureStatusEnum Constructor#
Initializes a new instance of the PLCamera.BslTemperatureStatusEnum class
PLCamera.BslTemperatureStatusEnum.Critical Property#
The temperature is close to or at the allowed maximum. Provide cooling.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB
PLCamera.BslTemperatureStatusEnum.Error Property#
The temperature is above the allowed maximum. Provide cooling immediately.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB
PLCamera.BslTemperatureStatusEnum.Name Property#
The full name of BslTemperatureStatus
PLCamera.BslTemperatureStatusEnum.Ok Property#
The temperature is within the normal operating temperature range.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress, boost_V_CoaXPress and dart 2 USB