PLCamera.ShaftEncoderModuleCounterModeEnum Class#
Applies to: CameraLink and GigE
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ShaftEncoderModuleCounterModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.ShaftEncoderModuleCounterModeEnum | Initializes a new instance of the PLCamera.ShaftEncoderModuleCounterModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
FollowDirection | The tick counter increases for forward ticks and decreases for reverse ticks. Applies to: CameraLink and GigE | |
IgnoreDirection | The tick counter of the shaft encoder module increases for forward ticks and for reverse ticks, i.e., the tick counts are incremented regardless of the direction of movement. Applies to: CameraLink and GigE | |
名前 | The full name of ShaftEncoderModuleCounterMode (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of ShaftEncoderModuleCounterMode (Overrides Object.ToString()()()().) |
PLCamera.ShaftEncoderModuleCounterModeEnum.ToString Method#
The full name of ShaftEncoderModuleCounterMode
Return Value#
Type: String
Returns the full name of ShaftEncoderModuleCounterMode
PLCamera.ShaftEncoderModuleCounterModeEnum Constructor#
Initializes a new instance of the PLCamera.ShaftEncoderModuleCounterModeEnum class
PLCamera.ShaftEncoderModuleCounterModeEnum.FollowDirection Property#
The tick counter increases for forward ticks and decreases for reverse ticks.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleCounterModeEnum.IgnoreDirection Property#
The tick counter of the shaft encoder module increases for forward ticks and for reverse ticks, i.e., the tick counts are incremented regardless of the direction of movement.
Applies to: CameraLink and GigE
PLCamera.ShaftEncoderModuleCounterModeEnum.Name Property#
The full name of ShaftEncoderModuleCounterMode