IBufferFactory Interface#
Syntax#
C#
VB
The IBufferFactory type exposes the following members.
方法#
名前 | 説明 | |
---|---|---|
AllocateBuffer | Allocates a buffer and provides additional context information. | |
FreeBuffer | Frees a previously allocated buffer. |
IBufferFactory.AllocateBuffer Method#
Allocates a buffer and provides additional context information.
Syntax#
C#
void AllocateBuffer(
long bufferSize,
ref Object createdPinnedObject,
ref IntPtr createdPinnedBuffer,
ref Object bufferUserData
)
VB
Sub AllocateBuffer (
bufferSize As Long,
ByRef createdPinnedObject As Object,
ByRef createdPinnedBuffer As IntPtr,
ByRef bufferUserData As Object
)
パラメーター#
- bufferSize
- Type: System.Int64
The size of the buffer in bytes that has to be allocated. - createdPinnedObject
- Type: System.Object
Underlying object (e.g., Array of bytes) that is used for providing createdPinnedBuffer. This object is provided when FreeBuffer() is called. - createdPinnedBuffer
- Type: System.IntPtr
Return the pointer to the allocated and pinned buffer. This pointer is provided when FreeBuffer() is called. - bufferUserData
- Type: System.Object
User data information that belongs to the buffer. This user data information is provided when FreeBuffer() is called. The value can be left unchanged if not needed.
Remarks#
Thread Safety: This method must be thread-safe.
Error Safety: Must throw an exception if the allocation fails.
IBufferFactory.FreeBuffer Method#
Frees a previously allocated buffer.
Syntax#
C#
VB
Sub FreeBuffer (
createdPinnedObject As Object,
createdPinnedBuffer As IntPtr,
bufferUserData As Object
)
パラメーター#
- createdPinnedObject
- Type: System.Object
The pointer to the allocated object. Created by this factory. - createdPinnedBuffer
- Type: System.IntPtr
The pointer to the allocated buffer. Created by this factory. - bufferUserData
- Type: System.Object
User data information of the buffer returned by AllocateBuffer(Int64, Object, IntPtr, Object).
Remarks#
Thread Safety: This method must be thread-safe.
Error Safety: Must not throw exceptions.