PLCamera.RemoveParameterLimitSelectorEnum Class#
Applies to: ace USB
Visibility: Guru
Selecting Parameters: RemoveParameterLimit
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.RemoveParameterLimitSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.RemoveParameterLimitSelectorEnum | Initializes a new instance of the PLCamera.RemoveParameterLimitSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
AutoTargetValue | The factory limits of the AutoTargetValue parameter can be removed. Applies to: ace USB | |
BlackLevel | The factory limits of the BlackLevel parameter can be removed. Applies to: ace USB | |
ExposureOverhead | The factory limits of the ExposureOverhead parameter can be removed. Applies to: ace USB | |
ExposureTime | The factory limits of the Exposure Time parameter can be removed. Applies to: ace USB | |
Gain | The factory limits of the Gain parameter can be removed. Applies to: ace USB | |
名前 | The full name of RemoveParameterLimitSelector (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of RemoveParameterLimitSelector (Overrides Object.ToString()()()().) |
PLCamera.RemoveParameterLimitSelectorEnum.ToString Method#
The full name of RemoveParameterLimitSelector
Return Value#
Type: String
Returns the full name of RemoveParameterLimitSelector
PLCamera.RemoveParameterLimitSelectorEnum Constructor#
Initializes a new instance of the PLCamera.RemoveParameterLimitSelectorEnum class
PLCamera.RemoveParameterLimitSelectorEnum.AutoTargetValue Property#
The factory limits of the AutoTargetValue parameter can be removed.
Applies to: ace USB
PLCamera.RemoveParameterLimitSelectorEnum.BlackLevel Property#
The factory limits of the BlackLevel parameter can be removed.
Applies to: ace USB
PLCamera.RemoveParameterLimitSelectorEnum.ExposureOverhead Property#
The factory limits of the ExposureOverhead parameter can be removed.
Applies to: ace USB
PLCamera.RemoveParameterLimitSelectorEnum.ExposureTime Property#
The factory limits of the Exposure Time parameter can be removed.
Applies to: ace USB
PLCamera.RemoveParameterLimitSelectorEnum.Gain Property#
The factory limits of the Gain parameter can be removed.
Applies to: ace USB
PLCamera.RemoveParameterLimitSelectorEnum.Name Property#
The full name of RemoveParameterLimitSelector